STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STemWin or TouchGFX for STM32 graphics?

I'm first working with GUIs and have some experience on bare-metal firmware programming for STM32 on SW4STM32. I'm studying both ways for GUI (TouchGFX and STemWin), but I can't understand all the pros and cons. Should I use TouchGFX for new projects...

JSilv.3 by Associate II
  • 7768 Views
  • 8 replies
  • 0 kudos

Resolved! Japanese text problem.

I have tried with Noto Sans, ipaexg, NotoSerifCJKjp-Medium. But still I am getting fallback character. I am using STM32H750VB. Can you please help how to fix this issue.

0693W00000Ba4xJQAR.jpg 0693W00000Ba4y1QAB.png 0693W00000Ba4xcQAB.png
RG.3 by Associate III
  • 8519 Views
  • 20 replies
  • 1 kudos

STM32F746IGT, &Inch Display & TouchGFX Problem.

Hai everyone ....,I am new to touchGFX, I have a STM32F746IGT based waveshare development board and 7 Inch display (800X480 Pixels) SDRAM with 16bit data bus from Micron,QSPI flash.I firstly try to configure LTDC to display a image on LCD from flash...

0693W00000BatrfQAB.jpg
GMano.1 by Associate II
  • 1535 Views
  • 3 replies
  • 0 kudos

Optimizing Framebuffer Fetching, Touchgfx

I am following AN4861, and reading 4.5.2.I have a 800x480 display, so I need the closest 64 byte multiple. 8321) In CubeMX, DMA2D-Basic Parameters- DMA2D Output Offset. (832-800) = 322) In CubeMX, Additional Software-TouchGFX Width(LTDC) = 832...

MEder by Associate III
  • 2080 Views
  • 4 replies
  • 1 kudos

Resolved! Image and Text quality is lost

Hi, For the application I am building in TouchGFX, the image and text quality is very good and crisp in developed screen. However, the quality/resolution is not retained in simulation. Below are the before and after pictures. In this picture, both th...

0693W00000AQ5KSQA1.png 0693W00000AQ5KhQAL.png
BGuth.1 by Senior
  • 2623 Views
  • 8 replies
  • 0 kudos

Debug Error with Touchgfx

Hi.board : stm32L4R9-EVALLCD : MB1315ATouchGFX version : 4.16.1STM32CubeMX : 6.2.1​I try to get index of scrollList selected.before add callback function, debugging is work.However If I add callback function, Debugging is Strange.(Some function is re...

0693W00000BarY7QAJ.jpg
Hben.1 by Associate
  • 1596 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.