STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Text Area word space set

Hi,I am doing layout and confused of changing the word space of a string? It seems that the designer doesnt support this operation./JJLin

JJ.Lin by Associate III
  • 1013 Views
  • 1 replies
  • 0 kudos

How to change screen from user code space?

Let say in Screen1 view I have custom widget widget1. In Widget widget1 upon certain user input, we want to switch to Screen2 view. How can we do this?Can we switch directly to Screen2 from widget1?Or widget1 has to propagate the user input to Screen...

BParh.1 by Senior III
  • 3972 Views
  • 3 replies
  • 2 kudos

Resolved! Bug in generated STM32DMA class on newest version 4.17.0

HelloJust as an information; (@Alexandre RENOUX​ )You added the function OSWrappers::taskYield() when using L8 images.TaskYield() is called in the function setupDataCopy. The problem: setupDataCopy is also called from ISR as you know, TaskYield() is ...

jimmii by Senior II
  • 5068 Views
  • 12 replies
  • 0 kudos

Why touch repeat button in touchgfx

Hi.i have a custom board and i made a touchgfx project.​everything works fine and my custom touch driver works good.but just a little situationWhen touch a button.button repeat quickly.every time that touchgfx function execute one time the button do ...

ajafa.1 by Associate
  • 1129 Views
  • 0 replies
  • 0 kudos

adding items to scroll at run time

This of this like an address book, where the user can add and delete people from it. The scroll wheel is on the first screen and it list everyone in the address book. When you click on a person there are feilds you can edit and save. or delete th...

jeff belz by Associate II
  • 1344 Views
  • 1 replies
  • 0 kudos

Resolved! "Generate Code" with TouchGFX - by using STM32H747 Discovery - folder "STM32CubeIDE" will be not created. Is it possible to use STM32CubeIDE for debugging with STM32H747?

If I press button "Generate Code" under TouchGFX: With STM32H747 Discovery board folder STM32CubeIDE is missing. But with board STM32H7B3 Discovery kit folder STM32CubeIDE will be created automatically and file ".Project" (for CubeIDE) is generated. ...

stmdelta by Associate II
  • 10529 Views
  • 19 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.