STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Interfacing FMC Display with STM32H743

What is the Max resolution supported in TouchGFX 4.17 with FMC display interface ? I am using a display with 800 x 480 resolution, will that work ? Display comes with a controller board using SSD1963 IC with 8080 / 6800 interface mode. Problem is tha...

VShet.2 by Associate III
  • 1643 Views
  • 0 replies
  • 0 kudos

The TouchGFXDesigner v4.17.0 will keep freezing

The TouchGFXDesigner v4.17.0 will keep freezing. The program does not respond to the mouse and keyboard. When you try to close the program, you are asked whether you want to save the changes, but you cannot do anything or select anything. In this sta...

OSole.1 by Associate II
  • 1638 Views
  • 2 replies
  • 0 kudos

Resolved! Successfully run in KEIL but failed to run in IAR.

I want to display 2 images in a screen, but it only display 1 image when used IAR to generate code. The project does not make any changes and generates code in KEIL, then it succeeds. (The code optimizations is none and CSTACK / HEAP space is large...

V.H by Senior
  • 2038 Views
  • 4 replies
  • 0 kudos

Resolved! The image gradually darkens

Hi, I want to make a big image gradually darken, I used setAlpha() and invalidate() function in handleTickEvent(), but frequent use of setAlpha() and invalidate() function slows down tick time.Is there a better way to implement this feature?

V.H by Senior
  • 974 Views
  • 1 replies
  • 0 kudos

n00b question: How big of a screen?

Trying to decide if TouchGFX with some variant of STM32H7 is the right solution for us and the Boss wants to know how big of a screen we can expect to drive and still get quality resolution and snappy feel. How do I determine memory requirements and ...

Use opencv on stm32

hi I was wondering if with libmjepg middolware it is possible to use opencv, and if it were which mcu interface should I use? thanks

SDall by Associate II
  • 2494 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.