STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to Instantiate a TouchGFX object dynamically?

Hi, I use TouchGFX in my HMI project, I want to create an instance of an object (ig. a button) in runtime (dynamically), so I could destroy it later and free it's allocation memory.I tried create it in a method but it seems to have runtime error:voi...

0693W00000D1nskQAB.jpg
amirparto by Associate II
  • 2680 Views
  • 3 replies
  • 3 kudos

disolay

HalloOn mipi display, touchgfx correct show menu, but its clock ans any png damaged. is way to correct it ?

DDom.1 by Associate II
  • 1387 Views
  • 1 replies
  • 0 kudos

Tearing effect and TouchScreeen Blocking

Hi All,I'm developping an custom board with an SPI Display (480x320 poixels).When I enable the TE pin on display and when I managed by Stm32 by interrupt,the touch screen stop to work because TouchControll::sampletouch(uint32_t x, uint32_t y)is no lo...

MPast.1 by Senior II
  • 1007 Views
  • 0 replies
  • 0 kudos

32F746GDISCOVERY TOUCH REPLACEMENT

Hi folks.Have broken with a hit the capacitive touch screen that covers the display. A big line has split the touch in two. One part is still responding the other one is dead.The board mounts an obscure LCD_Kunjian_ HT043C_40P_P080_FLEX_FOLDED accord...

SLa S.1 by Associate
  • 887 Views
  • 0 replies
  • 0 kudos

Resolved! QSPI SRAM as framebuffer and Parallel or MIPI DSI?

Hi,I have some questions regarding the implementation of an LCD with the STM32F479ii.The display we want to use, has a 800x480 resolution at 60Hz and can have either 16 or 24 bit color depth.A framebuffer for a display like that is of course not goin...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.