STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

I want to use touchGFX on STM32L496G-Disco with a screen connected to spi1 and not the on board screen.

I want to use touchGFX on STM32L496G-Disco with a screen connected to spi1 and not the on board screen.the screen connected to spi1 is supported on another board with the driver in ST7789.c + .h when it is connected to STM32L476RG_NUCLEO. the problem...

Eblec.1 by Associate II
  • 2603 Views
  • 8 replies
  • 0 kudos

How to get the screen transition status

Hi, I use 'makeTransition' function to animate the screen transition and the new screen has a large number of dynamic data display. I want to display these after transition finished, but how can get the status of screen transition (I checked file ...

V.H by Senior
  • 785 Views
  • 0 replies
  • 0 kudos

More indepth guide on programming TouchGFX?

Hey guys,So, I'm taking on a project that will use STM32H7 chip with a TFT panel screen (with touch capabilities) on a custom PCB. The project is a custom gauge (like a speedometer) that allow user inputs via the touch display. So my question is, doe...

Tnguy.3 by Associate III
  • 883 Views
  • 0 replies
  • 0 kudos

How to integrate custom touch controller with TouchGFX

Hi everyone!I'm trying to integrate my own touch controller with TouchGFX on a custom board. My touch driver gives me XY coordinates of an event (press or release). Basically with this information I can do whaterver I want. So, for example, I can cha...

nikof by Associate II
  • 1877 Views
  • 1 replies
  • 0 kudos

Resolved! Problem with bitmap caching touchGFX

Hi All,I have a problem with bitmap caching. Below is the contextProcessor and Peripheral’s details:-STM32F429ZITX micro8 Mega bytes external SD RAM16 Megabytes SPI flash(not quad)Our use case:- We have GUI application with several screens(setup , fu...

Kpodu.1 by Associate II
  • 7982 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.