STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Color problem on stm32h7

Hello, I am using my custom-developed STM32H7 PCB with an 800*480 TFT display connected via 24bpp RGB. Currently, I am only using external SDRAM (IS42S32800J) for the frame buffer, while my QSPI flash is inactive. For the configuration settings, I ba...

dumo by Associate
  • 1039 Views
  • 2 replies
  • 0 kudos

Resolved! Corrupted TouchGFX text

I have a TouchGFX application where Flex Button text is sometimes being corrupted as are TextArea widgets (both with and without Wildcards). Images remain unaffected. The processor is a STM32U599, display type is RGB888 LTDC based and no external FLA...

TouchGFX Text Corruption.png
dave2012 by Associate III
  • 1965 Views
  • 4 replies
  • 0 kudos

dynamicGraph Area image

Hello, I have no problem storing images in the MCU's internal flash, but when storing images to external flash, it enters HardFault_Handler(). This issue only occurs when calling dynamicGraph Area image, while other images can be read normally. Why i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.