2022-07-20 4:26 PM
hello
An error occurs about the screen deleted from TouchGFX.
I deleted a specific screen from TouchGFX and re-generated the code.
Also, CubeIDE also deleted the Cpp file corresponding to a specific sceen.
Then it builds normally.
However, the problem is that whenever Code Generation is performed in TouhGFX, the cpps deleted in CubeIDE are recreated and an error occurs.
Description Resource Path Location Type
fatal error: gui_generated/scrautoremain_i4_screen/ScrAutoReMain_i4ViewBase.hpp: No such file or directory STM32H735G-DK line 4 C/C++ Problem
make: *** [Application/User/gui/subdir.mk:243: Application/User/gui/ScrAutoReMain_i4Presenter.o] Error 1 STM32H735G-DK C/C++ Problem
make: *** [Application/User/gui/subdir.mk:245: Application/User/gui/ScrAutoReMain_i4View.o] Error 1 STM32H735G-DK C/C++ Problem
Every time TouchGFX does code generation, CubeIDE is in the process of building while deleting the CPP files corresponding to the previously deleted screens one by one.
I want to know the solution.
thank
Solved! Go to Solution.
2022-07-31 4:20 PM
hello,
I found the cause.
If there is a user-added code, it occurs as above, and the user-added code must be deleted in advance.
2022-07-21 1:43 AM
Hello @mSH.1 ,
I don't understand why you are deleting manually the cpp files corresponding to the screens in CubeIDE.
If you wanna get rid of a screen, just simply delete it in TouchGFXDesigner, and then press "Refresh" on the project in STM32CubeIDE, and try to rebuild it.
The screen files and references should be deleted then.
/Yoann
2022-07-31 4:20 PM
hello,
I found the cause.
If there is a user-added code, it occurs as above, and the user-added code must be deleted in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.