STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX Smart watch UI architecture design

Hi, Sorry for the long post, I was looking at the TouchGFX documentation for UI development and had some clarifying questions about the current active screen limitations.as well as general SW architecture questions.I'm looking into creating a smartwa...

DOkaz.1 by Associate II
  • 1334 Views
  • 0 replies
  • 0 kudos

Resolved! TouchGfx widget internet connectivity

Hi,I want to connect a display powered by TouchGFX to a PC via usb-c. Is it possible to allow internet connectivity for a GUI widget via the usb-c connection to the host PC?Thanks!

DOkaz.1 by Associate II
  • 4206 Views
  • 7 replies
  • 0 kudos

STM32H7 LTDC with high pixel clock 51.2Mhz

I have a 7" RGB LCD 1024x600 32bits framebuffer, the pixel clock is 51.2MHz for 60fps recommended in the datasheet.I tried to interface this LCD with an STM32H743i-EVAL2 board, which is working fine, until I began to try using 2 layers of 32bits (for...

CedricB by Associate II
  • 3267 Views
  • 1 replies
  • 0 kudos

Resolved! Checking memory usage

In the documentation, the file described is generated by IAR embedded workbench. I'm using cubeIDE. Where can I find the mapping file?

ksale.1 by Senior II
  • 2275 Views
  • 3 replies
  • 0 kudos

I had posted question regarding the Touch GFX and LwIP over STM32F7508DK. Has anyone such issue, Please community help me solve the issue. i have the attached the link below

https://community.st.com/s/question/0D53W00001hkRjCSAU/hello-im-facing-the-issue-with-touch-gfx-and-lwipi-generated-a-project-with-touchgfx-designer-opened-the-ioc-file-with-cubemx-and-added-ethernet-connectivity-along-with-the-lwip-stackwhen-i-creat...

LKade.1 by Associate II
  • 1563 Views
  • 2 replies
  • 0 kudos

DCMI to USB Video Streaming

Hi all!I need to transmit data captured from DCMI to USB as a UVC Device Class. Is there any existing example that works? I have verified the DCMI Interface and it works fine. Now I need to transfer the data over USB-HS. I am using STM32H747IIT6 as m...

Interfacing External Touch Sensor to Touch GFX Demo 2.

Hi Community,I wanted to interface external touch sensor to achieve following tasks.1) Slide to move the carousal icons.2) Touch to get into that particular application. Operations are happening with Touch Screen (STM32F769I-DISCO). I wanted to repla...

Vins by Senior
  • 1358 Views
  • 2 replies
  • 0 kudos

Gesture Events detection and handling

Hello,I am working on gesture events and getting a little bit confused.So, there is a method called sampleTouch that continuously checks if any new touch events are triggered (and used later on for example for click actions).So my question is:How to ...

AMS22 by Associate II
  • 1457 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.