STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Documentation of X-Cube Display

Hi allI'm planing to run a 16-bit TFT display with a NUCLEO U575 board. I already managed to get it running via FMC and a custom written library as stated in this thread. So the Display, the NUCLEO and the interface is running fairly well.However, as...

MGuth.1 by Associate III
  • 4004 Views
  • 5 replies
  • 0 kudos

STM32H747I-DISCO - screen burning.

It happened again, after changing some configuration in STM32CubeIDE ioc file. Breaking change, the application hanged with black screen for no apparent reason. As I tested with the debugger - it passes all initialization in main(), then hangs when s...

HTD by Senior III
  • 7321 Views
  • 8 replies
  • 2 kudos

Migrating from a project with an EVE2-based touchscreen to a Riverdi STM32H7-embedded screen, using TouchGFX

I have a working prototype using custom board with an STM32H7 controlling, among other things, a 7" FTDI-EVE2-based touchscreen. I wrote all the UI code using EVE2.I'm considering using TouchGFX to rebuild the UI and wonder about using a Riverdi scre...

APagl by Associate III
  • 917 Views
  • 0 replies
  • 0 kudos

Pink and green pictures in OV5640

Hi everyone Im tryng to capture RAW RGB pictures with ov5640 but all i get is pink and green ones. I asume im geting YUV pictures despite the configuration of format related registers is:format control (0x4300) = 0x00 (RAW, BGBG... / GRGR...)forma...

Egord.1 by Associate
  • 1471 Views
  • 1 replies
  • 0 kudos

sd card not working with touchgfx

Hi, I tried the example on formatting the sdcard and it works (https://www.youtube.com/watch?v=I9KDN1o6924).How do I implement this with TouchGFX? I set everything the same and mount the SD card (f_mount), but the next command is no longer executed (...

JNova.0 by Associate III
  • 1901 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.