STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Hardfault getText() when debugging

For writing to QSPI flash, I suspend the touchgfx thread. In debugging mode, I get sometimes a hard fault. I thought it comes from switching from and to memory mapped mode of the QSPI, but now I think the problem is somewhere else. The fault occurs a...

awiernie by Senior II
  • 1782 Views
  • 1 replies
  • 0 kudos

Resolved! setTypedText & Unicode::snprintf on the same textArea

i have a textArea called endPoint_Value which i would like to write both text from the TypeText ids using the setTypedText, but i also on different occations need to use the Unicode::snprintf & Unicode::snprintFloatThe textArea has a wildcard and buf...

New STM32F429I Discovery - Is my LCD damaged?

I just received my new STM32F429I Discovery board and I have uploaded the TouchGFX example.The LCD looks like clumsy at touch and the y axis is someway inverted.See my short video here (Unfortunately as new member I cannot add links, links are in the...

Fab64 by Associate
  • 2083 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.