STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Problem with the Project.

I got a problem when saving a TouchGFX project and open it with the CubeIDE.The first time I opened a proyect from TouchGFX with the CubeIDE, it looked like this.But then, when I do new proyects they look like this. I can't do anything and I tried un...

project one.png project 2.png
ferdlf by Associate III
  • 1482 Views
  • 2 replies
  • 1 kudos

Resolved! TextArea

How can I get the value from a textArea so I can compare it with this '-' character?

ferdlf by Associate III
  • 1539 Views
  • 2 replies
  • 2 kudos

Font rendering artifacts on TouchGFX 4.23

Hi, I decided to update TouchGFX in my project from 4.20 to the newest 4.23. I noticed some artifacts in font rendering from time to time. Below I attached a photo of the issue. Do you have any ideas why this is happening?Regards,Piotr

Image.jpeg
ypiotrp by Senior
  • 3638 Views
  • 4 replies
  • 0 kudos

Slider with inverted MIN, MAX values

Hello,I'm working with a slider and ran into this problem.When I definesetValueRange(0, 255);and then I set the valuesetValue(25);so everything works. But I would like to turn the values on the slider. That means I will entersetValueRange(255, 0);At ...

JNova.0 by Associate III
  • 1223 Views
  • 0 replies
  • 2 kudos

Resolved! Scroll animation

Does in the TouchGFX is scrollable container animation? I use doScroll() function but it would be nicer if it scrolls automatically with animation or smoothly.

heyo by Senior
  • 2922 Views
  • 3 replies
  • 0 kudos

Resolved! custom widget

Hello,once again the same question - Custom Widget.Everything I do now I do with a Custom Container, but I'm wondering how to do it with a Custom Widget.Can an existing widget be used in a custom widget? For example, can I draw a circle and a line un...

JNova.0 by Associate III
  • 2771 Views
  • 4 replies
  • 0 kudos

DynamicGraph issues

 I've been using dynamicGraph regularly by now (mostly in TouchGFX) and, randomly, in the generated code of both the .hpp and .cpp files (mainPageViewBase.hpp/.cpp) istances of elements inside the dynamicGraph are deleted/not generated (GraphelementD...

edsatt by Associate
  • 2432 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.