STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! start communication CAN if i press on Botton on touch GFX

Hello, in my project, I will be communicating via CAN with an STM32H735_G and a cluster of car components. I have a sequence of test examples. For exemple , if I send a specific frame to activate a feature within the car cluster, I aim to manage thes...

sana1 by Associate III
  • 1287 Views
  • 1 replies
  • 0 kudos

Touchgfx gets stucked in takeFrameBufferSemaphore()

Hello.During rapid screen switching, TouchGFX becomes stuck randomly in takeFrameBufferSemaphore().The issue reproduces within 1 hour after startup. We use TouchGfx 4.18.1 on STM32F439 and TouchGfx runs on external SDRAM. Also we have observed that  ...

Resolved! stm32f746g-disco, touchgfx

TouchGFX 4.15.0 and ST-LINK 4.6 and CubeProgram 2.6.0 installed to our system Windows 10 64Bit. Board Development STM32F746G Discovery.I'm tring to run touchgfx samples on the STM32F746G Discovery, every thing goes well and it seems code download com...

0693W000006EGG2QAO.jpg
AReza.1 by Associate II
  • 6825 Views
  • 11 replies
  • 1 kudos

Resolved! Direct access to screen on TouchGFX?

Hi,after reviewing answers to following posthttps://community.st.com/t5/stm32-mcus-touchgfx-and-gui/how-to-draw-pixel-line-or-rectangle/td-p/105737and as a TouchGFX newby, I'm wondering: how one expects to do a following task by using TouchGFX's:ther...

bear2023R by Associate III
  • 2419 Views
  • 4 replies
  • 2 kudos

Resolved! I want to use TouchGFX with stm32f207zgt6

Hello everyone in the community.I wanted to create a screen for "stm32f207zgt6" using "TouchGFX 4.23.1 Designer", but the board I wanted to use did not exist in the board options.How should I create a screen in this case?Also, after creating the scre...

t-oka by Associate III
  • 2887 Views
  • 4 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.