STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Unicode::snprintf string problem

Hi,I cannot seem to be able to print char array to unicode buffer.I have set Wildcard ranges to 0-9,A-z (also tried 0x20-0x7E)I'm trying to display file names in the UI, which have arbitrary and modifyable names. When I do snprintf with "%s" with a c...

Tuoman by Senior II
  • 8132 Views
  • 4 replies
  • 6 kudos

Resolved! Drawing a circle in a chess board

Hi!I want to ask a question about designing a chess game such as Gomoku using TouchGFX. As far as I know, I need to put two chesses in every single spot and set them as invisible. When user clicks, then set them to visible. However, this is a very te...

ZZY by Associate II
  • 2614 Views
  • 4 replies
  • 0 kudos

`FontFlashSection' will not fit in region `FLASH'

Hi all   I am coding based on STM32H735GDK. after I added a new font and debug on Touchgfx,  It showed wrong message : `FontFlashSection' will not fit in region `FLASH'   I uncommont the "FontFlashSection" in STM32H735IGKX_FLASH.ld to deploy the Font...

yuhui_1-1712282532823.png yuhui_0-1712282492494.png
yuhui by Associate II
  • 1887 Views
  • 2 replies
  • 0 kudos

Resolved! How to add additional c source file to TouchGFX project ?

Hey, my question is how to add additional c source files to TouchGFX project so I can build project in TouchGFX Designer?I know I have to edit Makefile . I already tried it but with no success. Here is the code of my makefile:# Helper macros to conve...

JLakn by Associate II
  • 6758 Views
  • 12 replies
  • 1 kudos

Resolved! GPU2D hangup on STM32H7S78-DK

Hello,I am experimenting on a STM32H7S78-DK board with a custom UI.Sometimes the board looks like frozen and inspecting with the debugger I always find that the core is running, but GUITask is waiting for nema semaphore.The call originates from nema_...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.