STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! QR Code Feature issue in TouchGFX 4.24

Hello , i am working for the first time on TouchGfx and learning step by step some basics about it . I currently encountred a problem with QR Code Feature . If i put an URL Link longer than 17 characters ,it wont be shown after i run the simulation ....

akdou by Associate
  • 1664 Views
  • 3 replies
  • 2 kudos

Resolved! How to use the circle progress?

Hi,I want to show a circle progress like below:In touchgfx's circleProgress, there is't the little circle at the progress line end;So I am drawing the little circle and update its position realtime;Is there any simpler way to do the same things?And m...

Junde_1-1729159898639.png
Junde by Senior III
  • 2006 Views
  • 3 replies
  • 1 kudos

Slow fade with touchgfx

I'm using touchgfx 4.22 on a stm32h755zi mcu. The touchgfx run on the M7 core. The mcu is running at 480MHz.The board is an internal board with a 800x480 display connected in parallel to the LTDC interface with a 18bit bus as shown below:I use an rgb...

LTDC.jpg Touchgfx conf.jpg DMA2D conf.jpg Fade.jpg
sbi by Associate III
  • 10563 Views
  • 14 replies
  • 9 kudos

Zephyr and TouchGFX?

So, have been using TouchGFX and FreeRTOS with the CubeIDE.  But, am looking into Zephyr because of the middleware (for things like networking including WiFi) it can pull in.  But I'm still going to need a GUI.Is anyone successfully using TouchGFX wi...

Jazman by Associate III
  • 5197 Views
  • 7 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.