2019-02-04 1:07 AM
Hello,
I'm a complete beginner of TouchGFX as I've just started exploring what it's got under the hood. I'm rather perplexed as to how I can access an element of a given screen from a container of said screen.
Let me elaborate. In the main screen, I've two containers C1 and C2. One (C1) that's invisible by default and that I'd like to render visible from a button click of C2. How can I accomplish that simply ? I'm sure it's straightforward but I don't know which function I've got to use for that. Note that both containers are statically loaded.
Thanks in advance
Solved! Go to Solution.
2019-02-05 1:49 AM
Hi @GMeur,
Here it is. A project that defines a screen with two custom containers (Both CustomContainer1). CustomContainer1 has a background and a ClickListener Box. When the Box is pressed, the CustomContainer catches this in an internal handler and then calls a Callback (set by the view) to communicate it's identity back. Based on this identity (The first or the second custom container) it will show/hide the custom containers.
I've written some comments in the code - Let me know if you need more information.
Best regards,
Martin
2019-02-04 2:37 AM
Hi @GMeur,
Screens have a root container that you add drawables to (Like Containers). The children are not aware of each other. What you want to do is have your C1 button call back to it's parent view and in that handler decide what to do. In this case, show C2.
I've already promised someone else i'd provide an example of how to make this coupling between containers and view. It's not something that's well integrated into the designer, sending arbitrary signals between elements. I will update this post once i get it done!
Hope that helps
Best regards,
Martin
2019-02-05 1:49 AM
Hi @GMeur,
Here it is. A project that defines a screen with two custom containers (Both CustomContainer1). CustomContainer1 has a background and a ClickListener Box. When the Box is pressed, the CustomContainer catches this in an internal handler and then calls a Callback (set by the view) to communicate it's identity back. Based on this identity (The first or the second custom container) it will show/hide the custom containers.
I've written some comments in the code - Let me know if you need more information.
Best regards,
Martin
2019-02-05 7:14 AM
Thanks. Very clear. It helps me a lot :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.