2022-06-13 9:56 PM
Hello,
We are working on interface of OV6946 camera with STM32F7508 development kit. We need to capture image and stream on STM32F7508 Display. Camera which we are using provides 10bit output with 400x400 resolution in Bayer’s format.
The connections are done as mentioned below:
Camera Pin Controller Pins
DCMI_D0 - PH9
DCMI_D1 - PH10
DCMI_D2 - PH11
DCMI_D3 - PH12
DCMI_D4 - PH14
DCMI_D5 - PD3
DCMI_D6 - PE5
DCMI_D7 - PE6
DCMI_D8 - PI1
DCMI_D9 - PI2
DCMI_PIXCLK - PA6
DCMI_HSYNC - PA4
DCMI_VSYNC - PG9
DCMI_SDA - PB9
DCMI_SCL - PB8
We are using example code from STM32 Cube example project named “Camera�?.
We are getting black and white scrolling image for the configuration given below
static void LCD_LL_ConvertLineToARGB8888(void *pSrc, void *pDst)
{
/* Enable DMA2D clock */
__HAL_RCC_DMA2D_CLK_ENABLE();
/* Configure the DMA2D Mode, Color Mode and output offset */
hdma2d_eval.Init.Mode = DMA2D_M2M_PFC;
hdma2d_eval.Init.ColorMode = DMA2D_OUTPUT_ARGB8888;
hdma2d_eval.Init.OutputOffset = 0;
/* Foreground Configuration */
hdma2d_eval.LayerCfg[1].AlphaMode = DMA2D_NO_MODIF_ALPHA;
hdma2d_eval.LayerCfg[1].InputAlpha = 0x00;
hdma2d_eval.LayerCfg[1].InputColorMode = DMA2D_INPUT_RGB888;
hdma2d_eval.LayerCfg[1].InputOffset = 0;
hdma2d_eval.Instance = DMA2D;
/* DMA2D Initialization */
if(HAL_DMA2D_Init(&hdma2d_eval) == HAL_OK)
{
if(HAL_DMA2D_ConfigLayer(&hdma2d_eval, 1) == HAL_OK)
{
if (HAL_DMA2D_Start(&hdma2d_eval, (uint32_t)pSrc, (uint32_t)pDst, 200, 1) == HAL_OK)
{
/* Polling For DMA transfer */
HAL_DMA2D_PollForTransfer(&hdma2d_eval, 100);
}
}
}
else
{
/* FatFs Initialization Error */
while(1);
}
}Please refer the link below for output reference:
https://drive.google.com/file/d/1ATyK06csLdJNzLO_H6x2dtP0buMR2cGr/view?usp=sharing
Please guide us, what are the built in configurations are need to be used for converting 10bit Bayer image input to RGB LCD output.
Thanks & Regards,
Ayaz Ahmed,
Riosh Technologies,
Bangalore.
2022-06-14 6:32 AM
Hi @NS.9 ,
The “Application note Digital camera interface (DCMI) for STM32 MCUs�? (AN5020), mentioned an example with RGB data capture.
I advise you to refer to this application note to resolve the problem.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-06-14 6:50 AM
The camera output is in raw Bayer format like below
How do we convert this to RGB format. We had referred the same document, can you please point out in the document where we can refer RAW data to RGB conversion.
2022-06-16 3:19 AM
We have successfully able to print color image on the display. But the Video streaming is scrolling vertically slowly.
Can you please share your view on this, what might be the cause for scrolling.
2022-06-16 4:13 AM
Hi @NS.9 ,
Glad to know that initial issue is already fixed.
Regarding the new issue: could you please share the code that can help to reproduce it so that I can investigate on my side?
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-06-21 10:02 PM
.
2022-06-22 12:36 AM
.
2022-06-26 11:26 PM
From the example code 'CAMERA' for STM32F7508-DK.
main.c/ "static void LCD_LL_ConvertLineToARGB8888(void *pSrc, void *pDst)" function we have configured DMA2D_Input_Color_Mode macro to DMA2D_INPUT_RGB888 and we are getting color image but the colors are not identical, in the place of yellow color we ara getting blue color and in the place of blue we are getting yellow color. This may be because of Bayer's color format. We tried all the macros mentioned below under DMA2D_Input_Color_Mode.
DMA2D_INPUT_ARGB8888 0x00000000U
DMA2D_INPUT_RGB888 0x00000001U
DMA2D_INPUT_RGB565 0x00000002U
DMA2D_INPUT_ARGB1555 0x00000003U
DMA2D_INPUT_ARGB4444 0x00000004U
DMA2D_INPUT_L8 0x00000005U
DMA2D_INPUT_AL44 0x00000006U
DMA2D_INPUT_AL88 0x00000007U
DMA2D_INPUT_L4 0x00000008U
DMA2D_INPUT_A8 0x00000009U
DMA2D_INPUT_A4 0x0000000AU
Can you please share the configuration for Bayer format.
2022-07-05 7:24 AM
@NS.9 has also started a separate thread on this:
2022-07-18 7:57 AM
It looks like there isn't real support for RAW Bayer in the DMA2D_Input_Color_Mode, as far as I can see. That's surprising, because the AN5020 clearly says it does. Maybe the hardware is capable but the code hasn't been written yet.
Can anyone confirm this?
Alternatively, you could of course use an older camera module with DVP (parallel) and RGB565 output support.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.