2021-03-22 8:48 PM
I'm following the security part 6 - 02 Building the SBSFU but the final build of the UserApp always ends up with an error.
Instructions are being followed EXACTLY as in the video. I'm getting a different project size when building the SBSFU, slightly larger at 59874 instead of 59578 as mentioned in the video and the documentation. Going on to the next step of building the UserApp will always fail with this error:
c:\st\stm32cubeide_1.0.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../../../../../../Projects/NUCLEO-L476RG/Applications/2_Images/2_Images_SBSFU/SW4STM32/STM32L476RG_NUCLEO_2_Images_SBSFU/Debug\se_interface_app.o: in function `SE_APP_GetActiveFwInfo':
(.SE_IF_Code+0x0): multiple definition of `SE_APP_GetActiveFwInfo'; ../../../../../../../../Projects/NUCLEO-L476RG/Applications/2_Images/2_Images_SBSFU/SW4STM32/STM32L476RG_NUCLEO_2_Images_SBSFU/Debug\se_interface_app.o:(.SE_IF_Code+0x0): first defined here
I'm running CubeIDE 1.6 and cube programmer 2.7 (tried with 2.5 as well). Will I need to downgrade Cube IDE as well?
2021-03-22 11:50 PM
Infact this is a regression with CubeIDE 1.6.0.
Workaround has been describe by my colleague Jocelyn here :
Sump up of the workaround :
1) Removing the -l:se_interface_app.o from Tools Settings/Libraries/Libraries
2) Adding the same -l:se_interface_app.o in Tool Settings/Miscellaneous/Other flags
2021-03-23 1:00 AM
That fixed it. Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.