2024-06-11 11:37 AM
Hello,
I would like to use the TFM application on STM32CubeIDE for the B-U585I-IOT02A board but I can't find the application anywhere. Any help?
Solved! Go to Solution.
2024-06-12 2:07 AM - edited 2024-06-12 3:07 AM
The TFM application for B-U585I-IOT02A is in the STM32 Cube U5 package available on st.com web site.
click on "Download latest version", unzip the zip file, the project is under Projects\B-U585I-IOT02A\Applications\TFM
Also if you downloaded it in STM32CubeMX it is in your user directory under c:\users\username\STM32Cube\Repository\STM32Cube_FW_U5_Vx.y.z
It is not present on ST's github (maybe due to some licensing problem ?)
2024-06-11 12:36 PM
Hello @Istillaga
I think you are tooking about the TFM example available on the X-Cube-AWS.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-12 12:45 AM
Hello @STTwo-32 ,
No, that's not the example I'm searching for. I am looking for the TFM application which is very similar to the SBSFU application.
2024-06-12 2:07 AM - edited 2024-06-12 3:07 AM
The TFM application for B-U585I-IOT02A is in the STM32 Cube U5 package available on st.com web site.
click on "Download latest version", unzip the zip file, the project is under Projects\B-U585I-IOT02A\Applications\TFM
Also if you downloaded it in STM32CubeMX it is in your user directory under c:\users\username\STM32Cube\Repository\STM32Cube_FW_U5_Vx.y.z
It is not present on ST's github (maybe due to some licensing problem ?)
2024-06-12 2:13 AM
Hello @Istillaga ,
TFM example is in the STM32CubeU5 here:
STM32Cube_FW_U5_V1.5.0\Projects\B-U585I-IOT02A\Applications\TFM\
It is not available in the GIT repo
Also be aware this is a quite old version of TFM : Version 1.3
TFM is not similar to SBSFU: TFM example includes SBSFU.
SBSFU is the secure boot
TFM example contains the same secure boot and provides the trusted firmware for Cortex-M implementation containing partition manager and different services such as secure storage and crypto.
When using SBSFU example only, the secure application is a very simple example of secure application. It is useful when you don't need the secure services provided by Trusted firmware for Cortex-M
Best regards
Jocelyn
2025-09-16 3:22 AM
Hi, I'm currently trying to find examples to start working on Secure boot and TFM on STM32U5 (I have a Nucleo-U575ZI-Q) but I can't find any examples or tutorial to start with. I'm trying to follow the UM2851 (https://www.st.com/resource/en/user_manual/um2851-getting-started-with-stm32cubeu5-tfm-application-stmicroelectronics.pdf) but I can't as I can't find the TFM application which it refers to.
I'm using STM32Cube IDE v1.19.0, with the package STM32Cube_FW_U5_V1.8.0.
Please can you help me ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.