2025-03-05 3:39 AM
Hello All,,
I am using STSAFE-A110 with stm32f429zit6 for secure boot, I want sample code / library for the same.
Also my another query is will I have to sign the firmware using openssl externally. can anyone provide me complete step to finish the secure boot.
Thanks in advance!!!!!
2025-03-10 4:49 PM
Hi @tobbymathew
can you take a look at STSAFE-A integration within OpenSSL security stack STSW-STSA110-SSL - STSAFE-A integration within OpenSSL security stack - STMicroelectronics
this discussion may also help you: Solved: STSAFE- A110 mqtt tls authentication - STMicroelectronics Community
Best Regards
2025-03-17 1:04 AM
Hi @tobbymathew,
For Secure Boot on STM32, please reference to the X-CUBE-SBSFU package.
You will find in the UM2262, the STSAFE-A is used only with STM32L4.
Regarding the firmware signing with OpenSSL, this will depends on the FW image you need to sign.
To generate a signature, you will need to use the openssl dgst feature with -sign to generate hash + signature of the image then, you will need to generate the full image with the signature.
Best Regards,
Benjamin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.