2021-03-26 2:15 AM
I'm working on creating a sfu loader to load sfb files from an external flash on a port I made for the STM32H735 (based on NUCLEO-H753ZI)
I follow the same steps as used in the ymodem loader:
It's at the last step that it fails during write. Writing the header succeeds however and using STM32CubeProgrammer I can verify the written data is correct.
The first chunk is 1024B and is written to address 0x08020400.
Looking into SFU_LL_FLASH_INT_Write() it turns out it fails on verification of the written data (if memcmp:(
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_FLASHWORD, destination, (source + i)) == HAL_OK)
{
/* Check the written value */
if (memcmp((void *)destination, (void *)(source + i), sizeof(SFU_LL_FLASH_write_t)) != 0)
{I added the following bit of code:
for (int ctr = 0; ctr < sizeof(SFU_LL_FLASH_write_t); ctr++) {
TRACE ("\r\n%02X %02X", *(uint8_t*)(source + i + ctr), *(uint8_t*)(destination + ctr));
}Which gives me
59 2800000
F4 2800000
33 2800000
C4 2800000
73 2800000
2A 2800000
75 2800000
...Then, trying to read that part of flash memory (0x08020000, 0x400B) using STM32CubeProgrammer I get an error Error: Data read failed but the option bytes all seem to be fine. No read or write protection is active (all SBSFU protections are disabled: SECBOOT_DISABLE_SECURITY_IPS is defined).
Any idea on what I'm missing?
Thank you.
Arno.
Solved! Go to Solution.
2021-03-26 10:34 AM
Hello Arno,
yes this is strange indeed.
As you made the porting from a 2 bank to 1 bank, I would suggest having a look to the STM32CubeFW H7 example in STM32Cube_FW_H7_V1.9.0\Projects\STM32H735G-DK\Examples\FLASH\FLASH_EraseProgram\ if not already done;
Also, I would recommend double checking your clocking/flash WS/ Voltage level
Best regards
Jocelyn
2021-03-26 7:16 AM
turns out the HardFault_Handler in sfu_low_level_flash_int.c is being triggered as well.
2021-03-26 7:55 AM
in the hard fault, the ecc flag is tested and seems to be set:
if (__HAL_FLASH_GET_FLAG(FLASH_FLAG_DBECCE_BANK1RR)/* || __HAL_FLASH_GET_FLAG(FLASH_FLAG_DBECCE_BANK2RR)*/)
{
TRACE("\r\n double ecc error \r\n");
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_DBECCE_BANK1RR);
// __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_DBECCE_BANK2RR);
/* Memorize error to ignore the read value */
DoubleECC_Error_Counter++;
...which seems strange because this is an almost brand new board (STM32H735G-DK).
2021-03-26 10:34 AM
Hello Arno,
yes this is strange indeed.
As you made the porting from a 2 bank to 1 bank, I would suggest having a look to the STM32CubeFW H7 example in STM32Cube_FW_H7_V1.9.0\Projects\STM32H735G-DK\Examples\FLASH\FLASH_EraseProgram\ if not already done;
Also, I would recommend double checking your clocking/flash WS/ Voltage level
Best regards
Jocelyn
2021-03-29 5:54 AM
Hi Jocelyn,
Thank you once more for your help!
Changing
p_erase_init.VoltageRange = FLASH_VOLTAGE_RANGE_3;to
p_erase_init.VoltageRange = FLASH_VOLTAGE_RANGE_4;did the trick. I also made sure to update SECoreBin- se_low_level.c with
p_erase_init.VoltageRange = FLASH_VOLTAGE_RANGE_4
Thank you again.
Best regards,
Arno
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.