cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U595 - Option Bytes not being Set after STANDBY or SHUTDOWN mode

KaiS_
Associate II

Hello,

I have a use-case with a soldered battery, which I can not power-cycle after programming, however I have to set option bytes to restrict Flash reading.

I found online that going into STANDBY mode or rather, returning from STANDBY mode, would update the option bytes. However, the option bytes are not set. Here is the relevant code block:

 

 

 

 

#if !defined(BOOTLOADER_DISABLE_AUTOLOCK)
  // Auto-enable RDP level 1 (JTAG readout protection)
  FLASH_OBProgramInitTypeDef option_bytes;
  HAL_FLASHEx_OBGetConfig(&option_bytes);
  if (option_bytes.RDPLevel != OB_RDP_LEVEL_1) {
	  printf("Incorrect RDP level detected, auto locking\n");

	  if (HAL_FLASH_Unlock() != HAL_OK) {
		  goto option_byte_panic;
	  }

	  if (HAL_FLASH_OB_Unlock() != HAL_OK) {
		  goto option_byte_panic;
	  }

	  option_bytes = (FLASH_OBProgramInitTypeDef) {
		  .OptionType = OPTIONBYTE_RDP,
		  .RDPLevel = OB_RDP_LEVEL_1
	  };

	  if (HAL_FLASHEx_OBProgram(&option_bytes) != HAL_OK) {
		  goto option_byte_panic; // Freeze
	  }

	  __HAL_RCC_PWR_CLK_ENABLE();
	  __HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_FLAG7);
	  HAL_PWREx_EnterSHUTDOWNMode();

	  HAL_FLASH_OB_Lock();
	  HAL_FLASH_Lock();

	  goto option_byte_success;

option_byte_panic:
	  while(1);
option_byte_success:
  }
#endif

 

. Pressing a button on the device will trigger WKUP7.

I verified that the devices goes to STANDBY and is woken up correctly by pressing the button. However, looking at the device using STM32CubeProgrammer, I can still see the option bytes being set to AA.

 

How can I resolve this issue?

 

Best regards

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Jocelyn RICARD
ST Employee

Hello @KaiS_ ,

I have checked it is working fine.

What you need to make sure is that you don't have a debugger feature activated that prevents from really entering in standby mode.

This can happen if you download your code with debugger for instance.

You can check DBGMCU register for that

Best regards

Jocelyn

 

 

View solution in original post

3 REPLIES 3
KaiS_
Associate II

Btw. I also tried 

HAL_PWR_EnterSTANDBYMode();

Instead of 

HAL_PWREx_EnterSHUTDOWNMode();

but it was showing the same behaviour.

Jocelyn RICARD
ST Employee

Hello @KaiS_ ,

I have checked it is working fine.

What you need to make sure is that you don't have a debugger feature activated that prevents from really entering in standby mode.

This can happen if you download your code with debugger for instance.

You can check DBGMCU register for that

Best regards

Jocelyn

 

 

KaiS_
Associate II

Hi Jocelyn,

Thank you very much, setting

DBGMCU->CR = 0x0;

before going to STANDBY/SHUTDOWN mode actually did the trick.

Best regards