2026-03-31 6:26 AM
After porting the application "STM32Cube_FW_U5_V1.8.0\Projects\B-U585I-IOT02A\Applications\SBSFU" to our own board we have everything operational apart from the ability to invoke the local loader in production mode (RDP2).
I have reverted to the original B-U585I-IOT02A board and project and have a similar issue so I am wondering if this is broken or we have misunderstood something. The loader can be invoked in TFM_DEV_MODE with RDP0 but not in production mode with RDP2. The SBSFU application runs fine.
Changes from the default STM SBSFU project settings we used to test this on B-U585I-IOT02A
1) In SBSFU_Boot project remove the TFM_DEV_MODE pre-processor symbol definition
2) In boot_hal_cfg.h >> #define TFM_TAMPER_ENABLE NO_TAMPER
3) In boot_hal_cfg.h >> #define #define TFM_OB_BOOT_LOCK 0
4) In flash_layout.h >> //#define MCUBOOT_PRIMARY_ONLY (definition commented out)
5) In flash_layout.h >> #define MCUBOOT_APP_IMAGE_NUMBER 2
6) In hardening.sh >> write_protect_secure="-ob...........BOOT_LOCK=0"
Any ideas?
Thanks in advance
2026-04-30 10:04 AM
Hello @horatiosdad ,
that is strange indeed.
To jump in the loader you use the user button after a reset ?
Then what happens ?
Did you try re-enabling the traces ?
Best regards
Jocelyn
2026-05-05 5:16 AM
Pressing the user button over a reset prevents the application from running. The LED doesn't flash and the ns-appli menu is not output.
Enabling logging results in the following single line
[INF] Flash operation: Op=0x0, Area=0x0, Address=0x0\r\n
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.