2021-03-10 9:28 AM
The code from the 1.16 example builds fine in the EWARM. It writes the source blocks to the terminal, but as I see in the debugger, it fails to encrypt the input block. That times out as it fails to return a HAL_OK status.
/* Start decrypting aCyphertext, the decrypted data is available in aDecryptedtext */
if (HAL_CRYPEx_AES(&CrypHandle, aCyphertext, AES_TEXT_SIZE, aDecryptedtext, TIMEOUT_VALUE) == HAL_OK)
{
/* Display decrypted Data */
Display_DecryptedData(CBC, 128, AES_TEXT_SIZE);
}
else
{
/* Processing Error */
Error_Handler();
}
I have read all the how-to info in the examples.
Has anyone else run into this issue and found a solution?
Solved! Go to Solution.
2021-03-10 9:35 AM
@par Hardware and Software environment
- This example runs on STM32L486xx devices.
- This example has been tested with a STM32L486ZG embedded on an
STM32L476G-EVAL board and can be easily tailored to any other supported
device and development board.
2021-03-10 9:35 AM
@par Hardware and Software environment
- This example runs on STM32L486xx devices.
- This example has been tested with a STM32L486ZG embedded on an
STM32L476G-EVAL board and can be easily tailored to any other supported
device and development board.
2021-03-10 9:40 AM
I have the STM32L476xx on my STM32L476G-EVAL board. That does not have the crypto processor, is that correct?
2021-03-10 10:06 AM
It doesn't have the cryp/hash unit enabled, it is probably the same die with either it fused off at the die test stage, or with a different mask in the set lacking metalization, etc related to the unit. ST doesn't disclose the exact methodology, but the parts coming in a without/with pairing ie L476/L486 or F767/F777
2021-03-10 10:11 AM
okay thank you!
2021-03-10 11:45 AM
It looks like twin models with and without crypto can be distinguished by checking that config register of a crypto thingy holds written value.
For example, below is a code we use to distinguish STM32H753 from 743.
Maybe the same will work for L486 vs 476.
-- pa
#ifndef STM32H753xx
#define STM32H753xx /* override! */
#undef STM32H743xx
#endif
#include "stm32h7xx_hal.h"
#include <stdint.h>
#include <stdbool.h>
// Return true if the MCU has crypto
// so this is H7 variant with crypto (ex. H753 vs H743)
bool H7_hw_crypto_test()
{
// Test if HASH->CR is writable
__HAL_RCC_HASH_CLK_ENABLE();
HAL_Delay(5);
HASH->CR = 0;
__DSB();
HASH->CR = 0x20; // set HASH_CR_DATATYPE=HASH_DATATYPE_8B
__DSB();
uint32_t u = HASH->CR;
bool y = ((u & 0x30) == 0x20);
__HAL_RCC_HASH_CLK_DISABLE();
return y;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.