2019-11-22 4:54 PM
Porting NUCLEO-H753ZI/Applications/1_Image to STM32H753.
This is running on STM32H753I-EVAL2 board.
The bootload can be done in 2 steps (download SBSFU.bin, then download UserApp.bin) or in 1 step (download SBSFU_UserApp.bin). The behavior is the same: bootload starts, detects userapp, tries to jump to userapp at 0x08020400. Then the system restarts...
= [SBOOT] SFU_BOOT_CheckApplySecurityProtections
= [SBOOT] System Security Check successfully passed. Starting...
==========================================
= (C) COPYRIGHT 2017 STMicroelectronics =
= Secure Boot and Secure Firmware Update =
==========================================
= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL
= [SBOOT] STATE: CHECK STATUS ON RESET
INFO: Last execution status before Reboot was: Verifying Fw Image status.
INFO: Last execution detected error was: No error. Success.
= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD
= [SBOOT] STATE: CHECK USER FW STATUS
A valid FW is installed in the active slot - version: 1
= [SBOOT] SFU_BOOT_SM_VerifyUserFwSignature: VERIFY USER FW SIGNATURE
= [SBOOT] SFU_BOOT_SM_ExecuteUserFw: EXECUTE USER FIRMWARE
= [FWIMG] SFU_IMG_LaunchActiveImg: slot_0=x08020000 offset=x400
= [SBOOT] SFU_BOOT_CheckApplySecurityProtections
= [SBOOT] System Security Check successfully passed. Starting...
---------------------
SECBOOT_CRYPTO_SCHEME is SECBOOT_ECCDSA_WITHOUT_ENCRYPT_SHA256
So the user app is not encrypted.
I have checked and rechecked system_stm32h7xx.c and linker scripts. Watchdog is not enabled. So I don't know what is causing the reset.
Thank you for the helps.
Solved! Go to Solution.
2019-11-24 2:10 PM
The TRACE output of SFU_BOOT_ManageResetSources is missing and might help.
Then try these steps
2019-11-24 2:10 PM
The TRACE output of SFU_BOOT_ManageResetSources is missing and might help.
Then try these steps
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.