2025-03-20 8:00 PM - last edited on 2025-03-21 5:42 AM by Andrew Neil
Can recognize the chip, but can not burn and read the flash problem. In this case, is the chip broken or the chip locked?
There is also a case that the chip can be identified as burning, but it cannot run the normal working program
2025-03-21 5:23 AM - edited 2025-03-21 5:25 AM
Is this a genuine programmer? The serial number "123456" is suspect.
Can you connect over SWD?
2025-03-21 5:43 AM
@TDK wrote:Is this a genuine programmer?
@leo12345678 - see:
In particular:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.