2022-10-11 7:32 AM
I'm creating a new lora project starting from STM32Cube_FW_WL_V1.2.0, application LoRaWAN_SBSFU_1_Slot_DualCore.
I reserved some space (from 0x0801A000 to 0x0801BFFF) for some configurations.
I modified the file mapping_fwimg.ld like below
.\STM32Cube_FW_WL_V1.2.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_SBSFU_1_Slot_DualCore\Linker_Common\STM32CubeIDE\mapping_fwimg.ld
/* Dwl slot #1 : (2 kbytes) */
SLOT_Blob_Dwl_1_start = 0x08002800;
SLOT_Blob_Dwl_1_end = 0x08002FFF;
/* Active slot #2 (92 kbytes) */
SLOT_Active_2_header = 0x0803F000;
SLOT_Active_2_start = 0x08003000;
SLOT_Active_2_end = 0x08018FFF;
/***** NVM FLASH Data *****/
/* WARNING: Symbols not used. The NVMS address is defined in lora_app.c */
LW_NVM_ROM_start__ = 0x0801A000;
LW_NWM_ROM_end__ = 0x0801BFFF;
/* Active slot #1 (60 kbytes) */
SLOT_Active_1_header = 0x0803F800;
SLOT_Active_1_start = 0x0801C000;
SLOT_Active_1_end = 0x0802AFFF;
When trying to read the LW_NVM_ROM_Region from the application, i got an hard fault due to an Memory Management Fault.
Finally i found out that the are from from 0x08018000 ==> 0x0801AFFF (12 kbytes) is protected:
.\STM32Cube_FW_WL_V1.2.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_SBSFU_1_Slot_DualCore\2_Images_SBSFU\CM4\Inc\sfu_low_level_security.h
/**
* @brief Region 4 - Enable the execution for active slot in unprivileged mode.
* Read only capability configured
* In addition to region 3, from 0x08004000 ==> 0x08017FFF (80 kbytes)
*/
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_RGNV MPU_REGION_NUMBER4
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_START FLASH_BASE
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_SIZE MPU_REGION_SIZE_128KB
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_SREG 0xC1U /*!< 128 Kbytes / 8 * 5 ==> 80 Kbytes */
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_PERM MPU_REGION_PRIV_RO_URO
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_EXECV MPU_INSTRUCTION_ACCESS_ENABLE
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_TEXV MPU_TEX_LEVEL0
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_B MPU_ACCESS_BUFFERABLE
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_C MPU_ACCESS_NOT_CACHEABLE
/**
* @brief Region 5 - Enable the execution for active slot in unprivileged mode.
* Read only capability configured
* In addition to region 4, from 0x08018000 ==> 0x0801AFFF (12 kbytes)
*/
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_RGNV MPU_REGION_NUMBER5
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_START ((uint32_t)0x08018000)
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_SIZE MPU_REGION_SIZE_16KB
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_SREG 0xC0U /*!< 16 Kbytes / 8 * 6 ==> 12 Kbytes */
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_PERM MPU_REGION_NO_ACCESS
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_EXECV MPU_INSTRUCTION_ACCESS_DISABLE
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_TEXV MPU_TEX_LEVEL0
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_B MPU_ACCESS_BUFFERABLE
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_C MPU_ACCESS_NOT_CACHEABLE
Now the question:
I cannot find a reason why this area should be not accessible in the example project.
Can i just remove this protection like this?
.\STM32Cube_FW_WL_V1.2.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_SBSFU_1_Slot_DualCore\2_Images_SBSFU\CM4\Inc\sfu_low_level_security.h
/**
* @brief Region 4 - Enable the execution for active slot in unprivileged mode.
* Read only capability configured
* In addition to region 3, from 0x08004000 ==> 0x08017FFF (80 kbytes)
*/
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_RGNV MPU_REGION_NUMBER4
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_START FLASH_BASE
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_SIZE MPU_REGION_SIZE_128KB
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_SREG 0xC1U /*!< 128 Kbytes / 8 * 5 ==> 80 Kbytes */
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_PERM MPU_REGION_PRIV_RO_URO
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_EXECV MPU_INSTRUCTION_ACCESS_ENABLE
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_TEXV MPU_TEX_LEVEL0
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_B MPU_ACCESS_BUFFERABLE
#define APP_PROTECT_MPU_FLASHEXE_ADJUST_C MPU_ACCESS_NOT_CACHEABLE
/**
* @brief Region 5 - Enable the execution for active slot in unprivileged mode.
* Read only capability configured
* In addition to region 4, from 0x08018000 ==> 0x0801BFFF (16 kbytes)
*/
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_RGNV MPU_REGION_NUMBER5
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_START ((uint32_t)0x08018000)
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_SIZE MPU_REGION_SIZE_16KB
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_SREG 0x00U /*!< 16 Kbytes / 8 * 8 ==> 16 Kbytes */
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_PERM MPU_REGION_PRIV_RW_URO
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_EXECV MPU_INSTRUCTION_ACCESS_DISABLE
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_TEXV MPU_TEX_LEVEL0
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_B MPU_ACCESS_BUFFERABLE
#define APP_PROTECT_MPU_FLASHEXE_ADJUST2_C MPU_ACCESS_NOT_CACHEABLE
2022-11-10 9:31 AM
Hello @G.Buldo
Sorry for such late answer.
Looking at the project I cannot see any reason why this region is protected.
I suppose this is something that comes from another mapping and was left here unintentionally ...
Best regards
Jocelyn
2022-11-11 5:55 AM
Thank you, this is what i expected.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.