2022-04-09 6:27 AM
I am working on STM32 crypto library and using STM32L433RC controller,
I am facing the issue of signature mismatching.
i have followed below steps
Step -1 Key generation using openssl tool for ECC256 curve
openssl ecparam -name prime256v1 -genkey -noout -out private-key.pem
openssl ec -in private-key.pem -pubout -out public-key.pem
read EC key
writing EC key
openssl ec -in private-key.pem -text -noout
read EC key
Private-Key: (256 bit)
priv:
cd:3d:64:7d:dd:33:d1:d3:db:91:f5:99:be:0e:b8:
6b:16:8e:b2:20:b7:1d:c8:16:db:81:d0:57:07:4e:
04:58
pub:
04:5a:bc:6d:ab:e3:38:64:25:86:79:2a:17:d8:8d:
09:ce:43:36:f6:a1:ba:2d:db:25:d6:6d:42:f6:7e:
a0:ea:3f:ba:85:fd:a4:10:08:15:ee:06:0e:d9:e4:
e7:44:50:82:4a:87:ea:46:74:8d:3e:33:a3:55:53:
6f:32:60:80:81
ASN1 OID: prime256v1
NIST CURVE: P-256
Step -2
Hash computation, sign and verify message file using openssl tool
Result is verify ok
Step -3
Importing private and public keys in STM32 project - Okay
Step -4 computation of hash and signing using library functions
cmox_hash_compute(CMOX_SHA256_ALGO,
Message, sizeof(Message),
Computed_Hash,
`` CMOX_SHA256_SIZE,
&computed_size);
cmox_ecdsa_sign(&Ecc_Ctx,
CMOX_ECC_CURVE_SECP256R1,
Known_Random, sizeof(Known_Random),
Private_Key, sizeof(Private_Key),
Computed_Hash, CMOX_SHA256_SIZE,
Computed_Signature, &computed_size);
The generated signature is differ from the signature generated using openssl.
how i can see content of generated signature in openssl
I am using the command of openssl "asn1parse -inform=der -in signature.txt" to see signatures in hex.
I am unable to understand why both data are not matching.
2022-04-20 12:03 PM
Hello @PGhat.2 ,
As you can see, ECDSA signature take a random number as input.
I guess openSSL is not providing a way to provide this random number and uses PC random.
So, the only way to check everything is ok is to check if signature is OK using public key
Best regards
Jocelyn
2022-04-20 12:22 PM
>>So, the only way to check everything is ok is to check if signature is OK using public key
Exactly, I don't think there's any guarantee that the signature will be the same for any instantiation, just that the out-n-back test where you check the integrity using the public key, and that authenticates the validity/viability on any system.
Also, I seem to recall a private key can have many viable public ones, for similar reasons.
The OP should get the OPENSSL to generate several signatures, and see if they are always the same, or not. If the random number generation is working, I'd expect each to be unique.
2022-04-21 9:35 AM
Hello @Community member ,
I'm far from being a crypto expert, but from my understanding:
1) ECC private key is a random value
2) ECC public key is the multiplication of this random value by the ECC curve generator
So, I guess we can have only one possible public key associated to a private key.
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.