2025-10-21 7:05 AM
Hello,
I’m working on STM32H7 firmware using the STM32 Cryptographic Library (CryptoLib) for firmware decryption.
I have the following scenario:
Firmware is encrypted with AES128-GCM.
Integrity and authenticity are verified separately using ECDSA + SHA-256.
I want to decrypt firmware using AES-GCM in counter mode (CTR) without relying on the GCM authentication tag.
My questions are:
Does AES-GCM in STM32 CryptoLib support CTR-only operation, bypassing the Galois-field authentication step?
If not, is there a recommended way to perform AES-CTR decryption using CryptoLib on STM32H7 without tag verification?
Are there any known limitations or caveats when skipping GCM tag verification in STM32H7 CryptoLib?
Thanks in advance for guidance.
@Jocelyn RICARD @Fred
Solved! Go to Solution.
2025-10-23 11:11 AM - edited 2025-10-23 11:12 AM
Hello @SSaiPrasad, and welcome to ST Community!
To answer your questions:
> Does AES-GCM in STM32 CryptoLib support CTR-only operation, bypassing the Galois-field authentication step?
AES-GCM is an authenticated encryption mode: it always expects to compute and/or verify the authentication tag as part of the operation.
> If not, is there a recommended way to perform AES-CTR decryption using CryptoLib on STM32H7 without tag verification?
Yes, you should use the dedicated AES-CTR mode provided by the CryptoLib under Middlewares\ST\STM32_Cryptographic\legacy_v3 folder.
This mode performs only the counter-mode encryption/decryption, with no authentication or tag involved.
> Are there any known limitations or caveats when skipping GCM tag verification in STM32H7 CryptoLib?
No known hardware or library limitations for AES-CTR mode on STM32H7
Best regards,
2025-10-23 11:11 AM - edited 2025-10-23 11:12 AM
Hello @SSaiPrasad, and welcome to ST Community!
To answer your questions:
> Does AES-GCM in STM32 CryptoLib support CTR-only operation, bypassing the Galois-field authentication step?
AES-GCM is an authenticated encryption mode: it always expects to compute and/or verify the authentication tag as part of the operation.
> If not, is there a recommended way to perform AES-CTR decryption using CryptoLib on STM32H7 without tag verification?
Yes, you should use the dedicated AES-CTR mode provided by the CryptoLib under Middlewares\ST\STM32_Cryptographic\legacy_v3 folder.
This mode performs only the counter-mode encryption/decryption, with no authentication or tag involved.
> Are there any known limitations or caveats when skipping GCM tag verification in STM32H7 CryptoLib?
No known hardware or library limitations for AES-CTR mode on STM32H7
Best regards,
2025-10-27 12:40 AM
Thank you for the clarification and detailed response. That perfectly answers my questions.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.