2020-11-02 9:59 PM
2020-11-02 10:44 PM
First insure the STM32L5 Nucleo is plugged on you PC ( and insure you don't have any other ST board connected).
Then you can check in Windows device manager in Ports(COM &LPT) -> You should see a STLink Virtual com port.
You can open a command windows and type those command :
cd c:\STM32SecuWS\Tools\teraterm\
StartTTPL5.bat
You should see some trace.
If it's still not working, let me know and I will set up a short team meeting to help you.
2020-11-02 10:59 PM
2020-11-02 11:18 PM
You issue is link to the fact windows doesn't found mode command.
Could you check this is present on your PC ?
In a command windos:
dir C:\windows\System32\mode.com
If it's present, check you windows Path variable to insure the "C:\windows\system32" is present .
An other workaround would be to put the absolute path in the 2 following scripts
C:\STM32SecuWS\Tools\teraterm\StartTTPL5.bat
and
C:\STM32SecuWS\Tools\teraterm\StartTTPL4.bat
change line 25 :
FOR /F "tokens=4 USEBACKQ" %%F IN (`C:\windows\system32\mode ^| find " COM"`) DO (
2020-11-03 12:32 AM
Thank you so much. The second one was my problem. "C:\windows\system32" was not in Path.
Sorry for taking your time. It was maybe my third question in internet forums all my life, because there is always the answer, when I search for it, but as there were not too many days to the workshop, I was in a hurry to make sure about everything.
Sorry again.
Have a nice day.
2020-11-03 12:34 AM
No problem at all, you're welcome. I hope you will enjoy the workshop !
2020-11-03 12:39 AM
Thank you. That is definitely a very useful workshop.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.