2025-06-02 10:43 AM - edited 2025-06-02 12:15 PM
Hi,
I would like to work with the security features of STM32H533RE microcontroller. For that,
1.Do I need to enable anything or install any libraries files in order to work with it.
2. If there is any example projects available?
3. The path for Installation and documents .
Please help me out.
2025-06-02 1:02 PM
There are a bunch of examples here. Several of them deal with security features. These can likely be loading with the Example Selector in CubeMX/CubeIDE
STM32CubeH5/Projects/NUCLEO-H533RE at main · STMicroelectronics/STM32CubeH5
2025-06-04 1:04 AM
2025-06-05 1:13 AM
Hi,
I will go through it. STM32H533RE Nucleo board i am using it does not support secure Manager. If that is the case, How would I store the keys such that i cant be accessible. Is it possible to generate the keys.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.