2014-10-24 2:18 PM
I want to use the CRC example of IAR ''ROM size save with CRC32 Note 52791'' from my Boot.
The problem is that the intvec area set on start of the APP ROM but don't get into the CRC calculation.Today I see that the intvec place on 0x184 bytes.Can I rely on it that it stay always this size(even when program change) because I can't see from the Boot the map of the APP, so I have to take it as a constant? #intvec-size-crc-stm32f2052014-10-24 4:25 PM
Not clear why you couldn't/wouldn't checksum them. They are architecturally defined for each chip, and expressed as DCD/.WORD directives in the startup_stm32f4xx.s file
See the Vector Table in the Reference Manual - ''Interrupt and exception vectors''2014-10-25 12:06 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.