2026-02-17 7:07 AM
Hello everyone,
I am working on a custom board based on the STM32U575RGT6 (1MB Flash). I am encountering a hard fault (SecureFault) during the initialization of the Non-Secure application after integrating the SBSFU.
Context:
Hardware: Custom board with STM32U575RGT6.
Initial Project: A working application using TrustZone active + FreeRTOS (generated via CubeMX). The Option Bytes were set to a default 50/50 split (Secure/Non-Secure).
Goal: Implement a Secure Boot / Firmware Update mechanism.
What I did:
I used the ST example for B-U585I-IOT02A as a reference.
I integrated SBSFU_Boot and SBSFU_Loader into my project folder.
I adapted the linker scripts (.ld), postbuild.sh, and flash_layout.h to match the 1MB Flash size of the U575RGT6 (vs 2MB on the B-U585I).
In my original application, I replaced the .ld files and startup_xx.s files with those provided in the SBSFU_Appli example.
Configuration:
To simplify debugging, I disabled Tamper, Write Protection (WRP), and HDP protection in SBSFU_Boot.
RDP Level is set to Level 0.
The Behavior: The project compiles and links successfully. After flashing:
The Bootloader starts correctly.
It jumps to the Secure Application.
The Secure Application jumps to the Non-Secure Application.
Inside the Non-Secure main():
HAL_Init() executes fine.
HAL_PWREx_EnableVddA() executes fine.
CRASH: When calling SECURE_RegisterCallback(SECURE_FAULT_CB_ID, (void *)SecureFault_Callback);, the system jumps immediately to SecureFault_Handler().
Debugging Info: It seems related to the Non-Secure Callable (NSC) region or a GTZC configuration issue, but I am stuck. Since I adapted the flash layout for 1MB, I suspect I might have messed up a boundary definition.
Has anyone faced a similar issue when porting the U5 SBSFU to a smaller flash variant?
Any help or pointers on where to look would be greatly appreciated.
Thanks in advance!
Solved! Go to Solution.
2026-02-18 2:08 AM
Hello @DJean.3 ,
Secure fault means you have an issue in your SAU configuration.
You need to check with debugger, when you are in the secure application the SAU area address range for first area.
This is where the Non secure callable address is setup using CMSE_VENEER_REGION_START and CMSE_VENEER_REGION_SIZE.
Then check when calling the SECURE_RegisterCallback if address is in the good range...likely not.
To do this, you will need to step in assembly and check register before the call.
Best regards
Jocelyn
2026-02-18 2:08 AM
Hello @DJean.3 ,
Secure fault means you have an issue in your SAU configuration.
You need to check with debugger, when you are in the secure application the SAU area address range for first area.
This is where the Non secure callable address is setup using CMSE_VENEER_REGION_START and CMSE_VENEER_REGION_SIZE.
Then check when calling the SECURE_RegisterCallback if address is in the good range...likely not.
To do this, you will need to step in assembly and check register before the call.
Best regards
Jocelyn
2026-02-19 3:05 AM
Following your advice regarding the SAU configuration, I performed a deep dive into the generated .map and .list files of both Secure and Non-Secure projects.
I have identified the root cause of the SecureFault: The Non-Secure application is not calling the correct address for the Secure Gateway Veneer due to a memory aliasing mismatch.
Here is the evidence:
The Issue: The Non-Secure linker sees the symbol defined at 0x0C02FCE8 inside secure_nsclib.o. Since the NS code is running in the 0x08 range, the linker considers 0x0C as "out of range" or a different memory space, and seemingly generates a local trampoline/stub at 0x080537F8 (which is inside the NS Flash, far after the actual Secure partition) instead of branching to the Non-Secure Alias of the Veneer.
The correct target address should be: 0x0C02FCE8 (Secure Address) - 0x04000000 (Alias Offset) = 0x0802FCE8.
My Configuration:
My Question: What is the standard/clean way in the SBSFU/STM32U5 ecosystem to tell the Non-Secure Linker that symbols imported from secure_nsclib.o (defined at 0x0C...) must be called via their Non-Secure alias (0x08...)?
I tried manipulating the Non-Secure linker script to define ROM_NSC at 0x0802FC80, but since the symbol address is fixed inside the .o object, the linker still struggles. Do I need a specific objcopy step to re-map the import library, or is there a specific GCC linker flag I am missing to handle this TrustZone aliasing automatically?
Thanks for your help!
2026-02-19 11:14 AM
you are right the matter was because i used
/*
// <e>Initialize SAU Region 1
// <i> Setup SAU Region 1 memory attributes
*/
#define SAU_INIT_REGION1 1
/*
// <o>Start Address <0-0xFFFFFFE0>
*/
#define SAU_INIT_START1 NS_CODE_START /* start address of SAU region 1 */
/*
// <o>End Address <0x1F-0xFFFFFFFF>
*/
#define SAU_INIT_END1 NS_CODE_LIMIT /* end address of SAU region 1 */
/*
// <o>Region is
// <0=>Non-Secure
// <1=>Secure, Non-Secure Callable
*/
#define SAU_INIT_NSC1 0
/*
// </e>
*/
/*
// </e>
*/
/*
// <e>Initialize SAU Region 4
// <i> Setup SAU Region 4 memory attributes
*/
#define SAU_INIT_REGION4 1
/*
// <o>Start Address <0-0xFFFFFFE0>
*/
#define SAU_INIT_START4 0x40000000 /* start address of SAU region 4 */
/*
// <o>End Address <0x1F-0xFFFFFFFF>
*/
#define SAU_INIT_END4 0x8ffffffe /* end address of SAU region 4 */
/*
// <o>Region is
// <0=>Non-Secure
// <1=>Secure, Non-Secure Callable
*/
#define SAU_INIT_NSC4 0
/*
// </e>
*/
/*
// <e>Initialize SAU Region 5
// <i> Setup SAU Region 5 memory attributes
*/
#define SAU_INIT_REGION5 1
/*
// <o>Start Address <0-0xFFFFFFE0>
*/
#define SAU_INIT_START5 0x60000000 /* start address of SAU region 5 */
/*
// <o>End Address <0x1F-0xFFFFFFFF>
*/
#define SAU_INIT_END5 0xfffffffe /* end address of SAU region 5 */
/*
// <o>Region is
// <0=>Non-Secure
// <1=>Secure, Non-Secure Callable
*/
#define SAU_INIT_NSC5 0
/*
// </e>
*/
/*
// <e>Initialize SAU Region 6
// <i> Setup SAU Region 6 memory attributes
*/
#define SAU_INIT_REGION6 1
/*
// <o>Start Address <0-0xFFFFFFE0>
*/
#define SAU_INIT_START6 0x0BFA0000 /* start address of SAU region 6 */
/*
// <o>End Address <0x1F-0xFFFFFFFF>
*/
#define SAU_INIT_END6 0x17f401fe /* end address of SAU region 6 */
/*
// <o>Region is
// <0=>Non-Secure
// <1=>Secure, Non-Secure Callable
*/
#define SAU_INIT_NSC6 0
/*
// </e>
*/now i use this
/*
// <e>Initialize SAU Region 1
// <i> Setup SAU Region 1 memory attributes
*/
#define SAU_INIT_REGION1 1
/*
// <o>Start Address <0-0xFFFFFFE0>
*/
#define SAU_INIT_START1 NS_CODE_START /* start address of SAU region 1 */
/*
// <o>End Address <0x1F-0xFFFFFFFF>
*/
#define SAU_INIT_END1 NS_ROM_ALIAS(TOTAL_ROM_SIZE) /* end address of SAU region 1 */
/*
// <o>Region is
// <0=>Non-Secure
// <1=>Secure, Non-Secure Callable
*/
#define SAU_INIT_NSC1 0
/*
// </e>
*/
/*
// <e>Initialize SAU Region 4
// <i> Setup SAU Region 4 memory attributes
*/
#define SAU_INIT_REGION4 1
/*
// <o>Start Address <0-0xFFFFFFE0>
*/
#define SAU_INIT_START4 0x40000000 /* start address of SAU region 4 */
/*
// <o>End Address <0x1F-0xFFFFFFFF>
*/
#define SAU_INIT_END4 0x4FFFFFFF /* end address of SAU region 4 */
/*
// <o>Region is
// <0=>Non-Secure
// <1=>Secure, Non-Secure Callable
*/
#define SAU_INIT_NSC4 0
/*
// </e>
*/
/*
// <e>Initialize SAU Region 5
// <i> Setup SAU Region 5 memory attributes
*/
#define SAU_INIT_REGION5 1
/*
// <o>Start Address <0-0xFFFFFFE0>
*/
#define SAU_INIT_START5 0x60000000 /* start address of SAU region 5 */
/*
// <o>End Address <0x1F-0xFFFFFFFF>
*/
#define SAU_INIT_END5 0x9FFFFFFF /* end address of SAU region 5 */
/*
// <o>Region is
// <0=>Non-Secure
// <1=>Secure, Non-Secure Callable
*/
#define SAU_INIT_NSC5 0
/*
// </e>
*/
/*
// <e>Initialize SAU Region 6
// <i> Setup SAU Region 6 memory attributes
*/
#define SAU_INIT_REGION6 1
/*
// <o>Start Address <0-0xFFFFFFE0>
*/
#define SAU_INIT_START6 0x0BFA0000 /* start address of SAU region 6 */
/*
// <o>End Address <0x1F-0xFFFFFFFF>
*/
#define SAU_INIT_END6 0x0BFA01FF /* end address of SAU region 6 */
/*
// <o>Region is
// <0=>Non-Secure
// <1=>Secure, Non-Secure Callable
*/
#define SAU_INIT_NSC6 0
/*
// </e>
*/and SECURE_RegisterCallback is called without error.
but i faced to new problem.
in non-secured main, calling the Start scheduler function osKernelStart(); make the application going to SecureFault_Handler
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.