2020-07-20 2:40 PM
I'm in the process of integrating the SBSFU into a project.
I got stuck when the decryption process seemed to hang.
After I got the SeCoreBin symbols loaded I realized that it was waiting for CPU2 to become active (specifically while waiting for FLAG_WAIT_CPU2_RDY to be set to 0)
To make sure the FUS version was up to date I flashed a known-working application firmware and used it to read the FUS version (which is 1.1.0). But I noticed that I had to call SHCI_C2_FUS_GetState(..) twice, which means that the wireless firmware was running on CPU2.
Is it a problem for SBSFU when the wireless stack is running on CPU2? If not, what could cause shci_notify_asynch_evt not being called?
A deadlock here would mean a bricked product, which is of course not acceptable.
Thanks in advance!
2020-07-20 2:56 PM
I can reliably reproduce this by installing a firmware that uses the Wireless Stack (Bluetooth Full).
When I install the SBSFU afterwards it will always hang after transmitting an image (using the stock YMODEM protocol) while decrypting ("New Fw Encrypted, to be decrypted").
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.