2025-09-01 10:48 PM - last edited on 2025-12-30 2:00 AM by ELABI.1
Hello.
I'm working with STM32H573.
I have a question related with the use of STSAFE-A110 for TLS. I have to authenticate also the client.
I've succeded stablishing TLS mutual authentication with HTTPS server and TCP server (different applications, not related) using this type of functions from NetxDuo with the correct data and test certificates:
/* TCP Server */
nx_secure_tls_session_create();
nx_secure_tls_ecc_initialize();
memset(&certificate, 0, sizeof(certificate)); // Server Local certificate
nx_secure_x509_certificate_initialize();
memset(&certificate_, 0, sizeof(certificate_)); // Client certificate
nx_secure_x509_certificate_initialize();
nx_secure_tls_local_certificate_add();
nx_secure_tls_trusted_certificate_add();
nx_secure_tls_session_start();
/* HTTPS */
memset(&certificate, 0, sizeof(certificate)); // Server Local certificate
nx_secure_x509_certificate_initialize();
memset(&certificate_, 0, sizeof(certificate_)); // Client certificate
nx_secure_x509_certificate_initialize();
nx_web_http_server_secure_configure(&HTTPServer, &nx_crypto_tls_ciphers,
crypto_metadata_server, sizeof(crypto_metadata_server), tls_packet_buffer, sizeof(tls_packet_buffer),
&certificate, &ca_list[0], 1,&remote_issuer[0], 1,remote_cert_buffer, sizeof(remote_cert_buffer));
nx_web_http_server_start(&HTTPServer);
What I want to achieve is the same functionality but instead of using my own certificate for local, use the one that STSAFE-A110 has that I cannot access.
I understand that I have use the option: NX_SECURE_X509_KEY_TYPE_HARDWARE when adding the certs, but I don't know if there is a 'direct' way of using the STSAFE-A110 API to achieve it.
Note: I have tested the STSAFE-A110 with the examples and it works fine.
Thank you.
2025-11-18 1:02 AM
I have tried approaching it in several ways:
The STSAFE-A110 does not have an RSA key but an ECDSA key, so I configured the HTTPS server and generated new keys to have a server running with TLS1.3. It works correctly.
The configuration change a bit:
/* Server */
memset(&certificate, 0, sizeof(certificate));
nx_secure_x509_certificate_initialize(&certificate, server_ec_cert_der, (USHORT)server_ec_cert_der_len, NX_NULL, 0, server_ec_key_der, (USHORT)server_ec_key_der_len, NX_SECURE_X509_KEY_TYPE_EC_DER);
/* Client */
memset(&trusted_certificate, 0, sizeof(trusted_certificate));
nx_secure_x509_certificate_initialize(&trusted_certificate, client_ec_cert_der, (USHORT)client_ec_cert_der_len, NX_NULL, 0, NULL, 0, NX_SECURE_X509_KEY_TYPE_NONE);
/* Server Config */
nx_web_http_server_secure_configure(
&HTTPServer,
&nx_crypto_tls_ciphers_ecc, // ECC table
crypto_metadata_server, sizeof(crypto_metadata_server),
tls_packet_buffer, sizeof(tls_packet_buffer),
&certificate,
&ca_list[0], 1,
&remote_issuer[0], 1,
remote_cert_buffer, sizeof(remote_cert_buffer));
nx_web_http_server_secure_ecc_configure(
&HTTPServer,
nx_crypto_ecc_supported_groups,
(USHORT)nx_crypto_ecc_supported_groups_size,
nx_crypto_ecc_curves);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.