2025-08-27 10:43 PM - edited 2025-08-27 10:45 PM
Hello,
I am working with Nucleo-STM32U385RG to implement the Root of Trust (Secure Boot) feature, following the wiki guide: https://wiki.st.com/stm32mcu/wiki/Security:How_to_start_with_OEMiRoT_on_STM32U3
My test environment is STM32Cube_FW_U3_V1.2.0.
During step-by-step testing, I faced two issues that I need help with:.
When I build OEMiRoT_Boot with EWARM IAR v9.32 + STM32U3 patch, the build finishes but throws an error during the postbuild.bat step.
The wiki doesn’t explain anything about postbuild in this step.
Still, I got a binary file, so I could continue the flow.
For comparison, I also tried with STM32H5 OEMiRoT_Boot build, but I encountered a very similar error: https://wiki.st.com/stm32mcu/wiki/Security:How_to_start_with_OEMiRoT_on_STM32H573_and_563%E2%80%93TrustZone_enabled#STM32CubeFW_provided_code_compilation
Error Log:
FAILED: E:/ST_CubeMx_Repository/Repository/STM32Cube_FW_H5_V1.5.0/Projects/STM32H573I-DK/Applications/ROT/OEMiROT_Boot/EWARM/STM32H573I-DK_OEMiROT_Boot/postbuild.stamp cmd.exe /C cd E:\ST_CubeMx_Repository\Repository\STM32Cube_FW_H5_V1.5.0\Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Boot\EWARM\STM32H573I-DK_OEMiROT_Boot && cmd /C "cmd /C E:\ST_CubeMx_Repository\Repository\STM32Cube_FW_H5_V1.5.0\Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Boot\EWARM\postbuild.bat" && copy /Y nul E:\ST_CubeMx_Repository\Repository\STM32Cube_FW_H5_V1.5.0\Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Boot\EWARM\STM32H573I-DK_OEMiROT_Boot\postbuild.stamp > nul run config Appli with windows executable ===== ===== Error occurred. ===== See "E:\ST_CubeMx_Repository\Repository\STM32Cube_FW_H5_V1.5.0\Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Boot\EWARM\\postbuild.log" for details. Then try again. =====
|
After building the "secure" and "nonsecure" applications, I reached the execution step:
https://wiki.st.com/stm32mcu/wiki/Security:How_to_start_with_OEMiRoT_on_STM32U3#Execution_of_the_installed_application
I could connect the Nucleo board via Tera Term, but the messages I see are different from the wiki screenshot.
Here is my terminal output:
| [INF] TAMPER Activated [INF] Flash operation: Op=0x0, Area=0x0, Address=0x0 [INF] Starting bootloader OEMiROT [INF] Checking BL2 NV area [INF] Checking BL2 NV area header [INF] Checking BL2 NV Counter consistency [INF] Consistent BL2 NV Counter 0 = 0x1000000 [INF] Consistent BL2 NV Counter 1 = 0x1000000 [INF] Consistent BL2 NV Counter 2 = 0x1000000 [INF] Consistent BL2 NV Counter 3 = 0x1000000 [INF] Swap type: none [INF] Swap type: none [INF] Swap type: none [INF] Swap type: none [INF] Starting validation of primary slot(s) [INF] verify counter 0 1000000 1000000 [INF] counter 0 : ok [INF] hash ref OK [INF] verify counter 1 1000000 1000000 [INF] counter 1 : ok [INF] hash ref OK [INF] verify counter 2 1000000 1000000 [INF] counter 2 : ok [INF] hash ref OK [INF] verify counter 3 1000000 1000000 [INF] counter 3 : ok [INF] hash ref OK [INF] Bootloader chainload address offset: 0x18000 [INF] Jumping to the first image slot |
How should I handle or fix the postbuild.bat error during OEMiRoT_Boot build (both STM32U3 and STM32H5)? Is this expected or is something missing in my setup?
Why is my terminal log different from the wiki example? Does this indicate a problem in my configuration, or is it still a valid behavior?
Any advice or guidance would be greatly appreciated.
Thanks in advance!
Solved! Go to Solution.
2025-09-04 7:24 PM
I had fixed bootloader build error myself.
It caused by path mismatch problem.
2025-09-04 7:24 PM
I had fixed bootloader build error myself.
It caused by path mismatch problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.