2023-02-06 7:15 PM
I set the start address about RAM is 0X20002000, and disable shared but execution.
Than, I set a function which data is 0x20002004 to change the protected data.
when system enter the function, it will reset.
2023-03-02 2:51 AM
Hello @yweic.1 ,
I suggest checking this application note AN4730. It should help!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.