cancel
Showing results for 
Search instead for 
Did you mean: 

I am trying STM32CubeExpansion_SBSFU_V2.4.0 with 2 Active images and 2 Download areas and assigned the LOcation in mapping_fwimg.icf. Code is building but i am getting error = "[FWIMG] Header of SLOT_ACTIVE_2 is not under the firewall protection"

DMira.11
Associate II

0693W00000ANle9QAD.pngPlease guide me how to add SLOT_ACTIVE_2 to firewall protection.

This discussion is locked. Please start a new topic to ask your question.
14 REPLIES 14

@Ons KOOLI​ I am waiting for the response...Please help

Hi @DMira.1​ ,

I raised your issue internally, and still waiting for response from the specific team.

Best Regards,

Ons.

Bubbles
ST Employee

Hi @DMira.1​ ,

while SBSFU 2-image code supports automatic configuration of up to 6 slots, you cannot have more than 3 slots of one kind automatically configured by the code. Please see the declarations in sfu_fwimg_regions.h

So while 3 active and 3 download works without any modification to the provided SBSFU, to actually get 4 slots of one kind you need to change the SBSFU code significantly. I believe it's possible to make it work in the end, but to be honest, I see no practical use for 4 active slots.

Kind regards,

J.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @JHOUD​ 

Thank you for response, I tried automatic configuration but ends with some error. I modified in  sfu_fwimg_regions.h as well... Facing same issue

@DMira.1​ Can you be more specific?

I need a lot more detail to reproduce your problem. What "some error"?

J.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.