2020-07-15 7:40 PM
I'm working with an STM32F04, and I'd like to change the option bytes so that my firmware can't be read back out after the device is programmed. I can tell from documentation I need to set the RDP byte to something besides 0xAA or 0xCC, but there isn't much about how to do this from the IDE.
Is there an option or a file I can edit in the STM32CubeIDE to modify the byte once my firmware is programmed?
Thank you!
Solved! Go to Solution.
2020-07-15 8:50 PM
The only way to do this in STM32CubeIDE is to add a separate section in the linker for your option bytes.
The easiest way to change them is probably in STM32CubeProgrammer or in your startup code. Just add a section that checks RDP and change it if necessary.
2020-07-15 8:50 PM
The only way to do this in STM32CubeIDE is to add a separate section in the linker for your option bytes.
The easiest way to change them is probably in STM32CubeProgrammer or in your startup code. Just add a section that checks RDP and change it if necessary.
2020-07-16 12:30 PM
Thank you! I just downloaded CubeProgrammer and this is exactly what I was hoping for - automatic programming and option byte modification. Hopefully this helps the next person - it's easy to get lost with all of the different IDE/ DFuse/ etc. tools available
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.