2018-05-11 12:39 AM
Hello,
we are are looking for a microprocessor or microcontroller with the following features:
o USB FS or ethernet connectivity, ( USB FS preferred)o high processing power >= 700MHz, multi core if possibleo secure and protected flash for our program binariesI understand, that high performance calculations and on chip flash don't match that well, but maybe somebody has heard of a solution for this dilemma?
One main point is that we need to have our firmware well protected. External flash solutions seem to fail on this requirement...Can somebody please give me a clue?
Thanks in advance!
Markus#secure-boot #performanceWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.