2020-06-17 4:03 AM
Hello,
I'm working on two ST Nucleo-F439ZI boards, and using the Eclipse based STM32 IDE for the development and deployment on the boards.
I'm using the CRYP module in DMA mode to carry out AES-CBC operations.
I've generated the main skeleton of the code using the code generator, and this is the relevant output:
void HAL_CRYP_MspInit(CRYP_HandleTypeDef* hcryp)
{
if(hcryp->Instance==CRYP)
{
/* USER CODE BEGIN CRYP_MspInit 0 */
/* USER CODE END CRYP_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_CRYP_CLK_ENABLE();
/* CRYP DMA Init */
/* CRYP_IN Init */
hdma_cryp_in.Instance = DMA2_Stream6;
hdma_cryp_in.Init.Channel = DMA_CHANNEL_2;
hdma_cryp_in.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_cryp_in.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_cryp_in.Init.MemInc = DMA_MINC_ENABLE;
hdma_cryp_in.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_cryp_in.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_cryp_in.Init.Mode = DMA_NORMAL;
hdma_cryp_in.Init.Priority = DMA_PRIORITY_LOW;
hdma_cryp_in.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_cryp_in) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hcryp,hdmain,hdma_cryp_in);
/* CRYP_OUT Init */
hdma_cryp_out.Instance = DMA2_Stream5;
hdma_cryp_out.Init.Channel = DMA_CHANNEL_2;
hdma_cryp_out.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_cryp_out.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_cryp_out.Init.MemInc = DMA_MINC_ENABLE;
hdma_cryp_out.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_cryp_out.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_cryp_out.Init.Mode = DMA_NORMAL;
hdma_cryp_out.Init.Priority = DMA_PRIORITY_LOW;
hdma_cryp_out.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_cryp_out) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hcryp,hdmaout,hdma_cryp_out);
/* USER CODE BEGIN CRYP_MspInit 1 */
/* USER CODE END CRYP_MspInit 1 */
}
}However, if I leave the `PeriphDataAlignment` to the default value, hence byte, when I `HAL_CRYP_Encrypt_DMA(...)` gets executed, the DMA job never ends. This is true both for mem-to-periph and periph-to-mem, I checked this using the callbacks `HAL_CRYP_OutCpltCallback(...)` and `HAL_CRYP_InCpltCallback(...)`.
For example, when settings both to byte alignment, nothing happens, while when setting the input channel (mem-to-periph) to word alignment, the first step finishes, and the second (periph-to-mem) hangs indefinitely.
This does not happen when using the polling version `HAL_CRYP_Encrypt(...)`.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.