2016-08-29 11:46 AM
Hi all,
In the they instruct to fill unused ROM with 0xFF, is is arbitrary or is there some logic to it? The reason I ask is that if I fill it with 0x00 (as the erase flash value is) I don't have to waste time programming empty space in bootloader update. I leave the ROM range at max in theIELFTOOL tool (and bootloader crc verification function) because I have no idea how large the application might be in the future.
Thanks #ielftool-checksum-stm32 #crc2016-08-30 2:09 AM
Hi Clonimus74,
Check the of IAR SYSTEMS which describes how to calculate CRC32 in STM32hardware.-Hannibal-2016-08-30 2:26 AM
The link you shared is the same one I put in the OP, and it doent answer my question.
Is filling the unused flash area with 0xFF is arbitrary or is there a reason not to use 0x00 which is the value it has after erase operation (in STM32L151)? [so to simplify the bootloader process].We’re moving the ST Community to a new platform to give you a better and more reliable community experience.