2024-05-15 11:05 PM
Hello,
I have NUCLEO-U575ZI-Q board and I have followed the steps to generate an SFI file from the video "STM32Trust Video Series: X-Cube-SFI Part 3-Out-of-the-box". I managed to generate the SFI file correctly but when I tried to install the firmware, I got an error (when running the script FlashSFI_SWD_OEM_Dev.bat script at minute 16:00 in the video).
Now, when I try to connect the board to the STM32CubeProgrammer, I get the following error:
Error: ST_LINK error (DEV_TARGET_NOT_HALTED)
Now I can't connect the board to the STM32CubeProgrammer. What should I do now?
Solved! Go to Solution.
2024-05-17 9:44 AM
Hello @mikel-m ,
to recover your board you should set BOOT0 to VDD.
If you used a B-U585I-IOT02A you can use SW1 for this.
Then you will be able to connect with programmer in hot-plug mode.
Set first RDP Level 1 (0xDC) and apply
Then set RDP Level 0 (0xAA) and untick TZEN and apply
Best regards
Jocelyn
2024-05-17 9:44 AM
Hello @mikel-m ,
to recover your board you should set BOOT0 to VDD.
If you used a B-U585I-IOT02A you can use SW1 for this.
Then you will be able to connect with programmer in hot-plug mode.
Set first RDP Level 1 (0xDC) and apply
Then set RDP Level 0 (0xAA) and untick TZEN and apply
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.