2011-01-12 4:46 AM
2015-11-21 5:39 AM
So you pick the guy who's post count to the forum is ONE, and hasn't posted in TWO years?
Yes, it doesn't look like he sets crc_reg in that case, probably want a crc_reg = CRC->DR Seem to think I posted a working example earlier in the thread, where it does the last byte in software. But the purpose of writing crc_reg back into the register is that it causes the math to zero it out. Please don't use the U and Ur abbreviations, you're not texting2015-11-30 1:21 PM
It looks like it depends on which part you have for bit reversal and unit sizes. This is from the app note:
I'm using the F4 part and I need byte support so it looks like the hardware doesn't quite cut it.2015-11-30 3:53 PM
Yes, the F4/F2/F1 implementation is somewhat restrictive, but both the M3/M4 cores have a bit reversal instruction. So groups of 4 bytes can be handled directly, and the trailing bytes managed separately.The F3/F0 parts have a more flexible solution.
https://community.st.com/0D50X00009XkgXtSAJ
Edit: Fixed broken link, original post from 20-Oct-2015
2016-09-06 9:49 AM
Dear clive, please point me what i am doing wrong. The problem isdifferent CRC on PC and MCU.
//Calculate CRC using hardware stm32 crc modul
for
(i=4; i<64; i= i+4){
CRC->CR |= CRC_CR_RESET;
memcpy
(&temp_32, &UserRxBufferFS[i], 4);
CRC->DR = temp_32;
//Wrong as PC value
}
//PC side (visual studio). I use your function.
uint32_t i;
CRC_result = 0xFFFFFFFF;
for
(i=4; i<64; i = i+4){
memcpy
(&temp_32, &Output[i] , 4);
CRC_result = Crc32Fast(CRC_result, temp_32);
}
DWORD
Crc32Fast(
DWORD
Crc,
DWORD
Data)
{
static
const
DWORD
CrcTable[16] = {
// Nibble lookup table for 0x04C11DB7 polynomial
0x00000000,0x04C11DB7,0x09823B6E,0x0D4326D9,0x130476DC,0x17C56B6B,0x1A864DB2,0x1E475005,
0x2608EDB8,0x22C9F00F,0x2F8AD6D6,0x2B4BCB61,0x350C9B64,0x31CD86D3,0x3C8EA00A,0x384FBDBD };
Crc = Crc ^ Data;
// Apply all 32-bits
// Process 32-bits, 4 at a time, or 8 rounds
Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
// Assumes 32-bit reg, masking index to 4-bits
Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
// 0x04C11DB7 Polynomial used in STM32
Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
return
(Crc);
}
2016-09-06 11:15 AM
Resetting in every iteration of the loop is probably not helpful.
Suggest you provide a test vector of the data you are pushing through the CRC and the data you are seeing on the PC and MCU side.2016-09-07 11:59 PM
THank you! Now it works fine!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.