2024-01-21 10:49 PM
Hi all,
One small doubt on the tamper configuration, is it possible to configure both active and Passive tamper in the Same project/API, or both should be in different project/API. why this doubt is as Seed is not required for Passive tamper, so does it effect the passive tamper implantation if we implement in the same project.
Solved! Go to Solution.
2024-01-22 1:43 AM
Hi @meghasb,
yes, as long as you assign them to different pins, you can combine active and passive tamper in the same project. If you need more specific answer, you need to ask more detailed question.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-22 1:43 AM
Hi @meghasb,
yes, as long as you assign them to different pins, you can combine active and passive tamper in the same project. If you need more specific answer, you need to ask more detailed question.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-22 1:46 AM
@Bubbles Thanks.
2024-02-01 10:00 PM
Hi Bubbles,
Thanks for the reply, i have assigned the static tamper to pin PC13 and Dynamic to PE5-PE6, PA0-PA1. when I'm trying to run the code indusial for static, it detecting, and when I'm running with both(static and dynamic) in one project, static tamper is not triggered or no response from that. is their any configuration setting to be done in the tool?
2024-03-01 6:06 AM
Hi @meghasb,
what device are you using?
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-03 9:09 PM
Hi @Bubbles
Thanks for the reply, i'm using STMU585 controller.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.