2025-03-19 12:57 AM
Hello there,
I am practicing with the STM32H573I-DK demo board, STiROT demo project and the chain of certificate feature.
I have built a chain of certificates as described in https://wiki.stmicroelectronics.cn/stm32mcu/wiki/Security:How_to_start_with_STiRoT_on_STM32H573.
It seems that I cannot execute a regression a regression or other action by supplying the INTERMEDIATE key and certificate. For Instance, Full regression works with ROOT or LEAF credentials, but not the INTERMEDIATE.
Am I doing something wrong ? or is it that intermediate certificates are only meant to generate leaf certificates, and cannot be used to re-open a device.
Thanks for your feedback.
Christian
Solved! Go to Solution.
2025-03-19 1:06 AM
Dear @CRE
You're right the intermediate certificate purpose is to delegate the capacity to create leaf certificate.
This one can't be used to re-open or regress a device.
In the MOOC about secure manager we also describe the certificate chain:
https://www.youtube.com/watch?v=BOBXqUg-PQs&list=PLnMKNibPkDnF5QuZDba2fd2mhOBb0huJK&index=7
Best regards,
Frantz
2025-03-19 1:06 AM
Dear @CRE
You're right the intermediate certificate purpose is to delegate the capacity to create leaf certificate.
This one can't be used to re-open or regress a device.
In the MOOC about secure manager we also describe the certificate chain:
https://www.youtube.com/watch?v=BOBXqUg-PQs&list=PLnMKNibPkDnF5QuZDba2fd2mhOBb0huJK&index=7
Best regards,
Frantz
2025-03-19 2:28 AM
Thanks Frantz for the clear and fast answer,
I also had this question on the same topic: When you generate a certificate with the Trusted Package Creator, you actually get 2, like something.b64 and something_chain.b64. Cert_intermediate_chain.b64 is used later to generate leaf certificates, and cert_leaf_chain.b64 to re-open a device.
But what is the purpose of the other certificates, without "chain" in their names ?
Best regards,
Christian
2025-03-19 2:33 AM
@CRE,
"what is the purpose of the other certificates", in fact this is somehow an intermediate file but that can't be use to reopen the device. As the "chain" is composed of all the needed certificate.
Best regards,
Frantz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.