2025-10-29 3:26 AM - edited 2025-10-29 3:26 AM
I’m working with a NUCLEO-H533RE board (STM32H5 series, TrustZone enabled) and using ST-LINK for debugging.
Here is the issue:
Error: Unable to get core ID
Error: Cannot connect to access port 1! If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode. If you are trying to connect to a device which supports Debug Authentication with certificate and password, please open your device using it.SDMAuthenticate: Authentication successful
Debug Authentication Success
Disconnected from device.
ST-LINK FW: V3J16M8
Board: NUCLEO-H533RE
Voltage: 3.28VI've tried:
Still, after authentication, I cannot connect to the core or AP.
Questions:
Any guidance or known working configuration for STM32H5 with Debug Authentication would be appreciated!
2025-10-30 2:09 PM - edited 2025-10-30 2:15 PM
Hello @elby0
Welcome to the Community.
Maybe this post could be helpful to you: stm32h533 production state closed firmware not running.
Implementing debug authentication on STM32H5 using CLI tools
2025-11-11 6:37 AM
Hello @elby0 ,
There shouldn't be any issue. At least I've never seen such behaviour.
Did you manage to recover?
Best regards
Jocelyn
2025-11-11 6:44 AM
Hello @Jocelyn RICARD
No not yet. I still have the same issue. I didn't look at this in the last few weeks as I had other priorities but I will get back to you when I have the chance to look into this.
Regards
elby
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.