STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Installing ST Cube Crypto Library fails on STM32CubeMX 4.11.0

Posted on November 11, 2015 at 18:11I'm trying to install the STM32Cube Cryptographic Library v3.0.0 on a fresh STM32CubMX install, version 4.11.0, under Windows 7. Installation fails with a message that ''This Package version is not managed on this...

Steve H by Associate III
  • 1700 Views
  • 2 replies
  • 0 kudos

About CRC

Posted on October 30, 2015 at 20:08Hi. I want to make SSI protocol with SPI peripheral on STM32F3 series. Also want to use DMA for Tx. There is a hardware CRC calculation unit, which calculate CRC above all data and is attached as last byte (in my c...

matic by Associate III
  • 1141 Views
  • 2 replies
  • 0 kudos

Disabling Flash readout protection through sram

Posted on October 06, 2015 at 12:24Hi all, Anyone knows why the following code is not disabling the flash memory readout protection? It is being executed on a STM32F103 microcontroller.FLASH_Unlock();  FLASH_ReadOutProtection(DISABLE);  FLASH_UserOp...

carles by Associate
  • 1126 Views
  • 1 replies
  • 0 kudos

sha-1 problem with stm32 crypto lib

Posted on June 14, 2015 at 15:15Hi,I'm developing on the stm32f207 with the M3_CryptoFW_RngHW_2_0_6.libI would like to use the sha-1 from lib but from some reason I do not get the correct result.Here is my test...My input buffer is 8 bytes: 1,2,3,4,...

ari_v2 by Senior
  • 4399 Views
  • 8 replies
  • 0 kudos

STM32 crypto library

Posted on May 19, 2015 at 12:47I am trying out some examples of the crypto library from ST, but its not working the way it should.If I try the AES-CBC192 examples on a STM32F107 (STM3210C eval board),I can verify that the encrypted cipher text is co...

0690X00000605E3QAI.png
brj2 by Associate II
  • 1402 Views
  • 1 replies
  • 0 kudos

Wrong CRC on STM32F3 at byte-level

Posted on April 08, 2015 at 13:09I'm trying to use the CRC peripheral on STM32F3 to calculate the CRC at byte-level but I can not get the same result as indicated in application note AN4187. The following snippet of code should return a CRC equal to...

RDP level1 is automatically SET on STM32F407 ! STRANGE ISSUE!

Posted on October 16, 2014 at 17:32Hi all,I have a very strange issue with STM32F407ZG; sometimesthe RDP level 1 is automatically set and then using STLink Utilities I can goback to RDP level 0.BUT, Now I get RDP level 1 SET and I can't go toRDP lev...

moez by Associate II
  • 6925 Views
  • 17 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.