STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do you generate public and private keys for RSA?

The user manual (UM1924) says in section 15 RSA Algorithm:There are two structures that pass keys to the functions:•RSAprivKey_stt for the private key•RSApubKey_stt for the public keyAll members of the above functions should be filled by the user bef...

MMart.9 by Associate II
  • 2193 Views
  • 2 replies
  • 0 kudos

Resolved! Port the SBSFU to STM32F730 in XiP mode

Hi, I just went over the X-Cube-SBSFU material and tried to compile the example projects to get an overall picture of this function.The MCU I used is STM32F730I8 and I am using the STM32F7308-DISCO board.As only 64kB flash is available in STM32F730 s...

JYeh.9 by Associate III
  • 3648 Views
  • 8 replies
  • 0 kudos

CRC16 for STM32F030

I am trying to use the hardware peripheral on the STM32F030 to calculate a 16-bit CRC for a modbus RTU application. But I don't know how to do it.

Yq by Associate
  • 2638 Views
  • 3 replies
  • 0 kudos

Resolved! How to implement AES using the Cryptographic processor?

The reference manual gives a brief description but how do you actually implement it?I'm using an STM32F437 which includes a cryptographic accelerator so I'm not looking to use the Cryptographic Library.Any documentation, tutorial, example code or any...

MMart.9 by Associate II
  • 1676 Views
  • 2 replies
  • 0 kudos

AES HW Timeout Crypto Lib

Hi,In my company we are currenlty looking at integrate the crypto lib.I have created a small STM32 IDE project to test the crypto lib provided by ST. I am using the Nucleo STM32413. The whole project compiles and I can succesfully call AccHw_AES_CFB_...

ABern by Associate II
  • 1536 Views
  • 2 replies
  • 0 kudos

RDP level 1 flash protection on STM32H753

Hello,When the RDP level 1 protection option bytes is set and the boot adress is set in the user flash memory, what are the debugger protections ? Which parts of the microcontroller still remain available via the JTAG debug port or the SWD debug po...

YROSS by Associate II
  • 1059 Views
  • 0 replies
  • 1 kudos

STM32 Security Issues

According to following white paper, some STM32 MCUs has security issues.https://www.usenix.org/system/files/conference/woot17/woot17-paper-obermaier.pdfThe question is Which STM32 components are affected?We are considering to use STM32H750vb and STM3...

MMagl by Associate III
  • 913 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.