STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with USB Virtual COM After SBSFU on STM32WB55RG

Hello everyone,My team and I are working with a custom board based on the STM32WB55RG. Due to limited pin availability, we need to use USB as a virtual COM port for serial communication. We successfully configured the USB Virtual COM and were able to...

G_P by Associate II
  • 3570 Views
  • 9 replies
  • 4 kudos

Resolved! Enable RDP after UART dfu

Hi,we are experiencing an issue with the STM32G0B0 when RDP level 1 is enabled, following the steps below:Flash the device using J-LinkStart the device and let the application set RDP = 1Enter the STM32 ROM bootloader (via UART)Disable RDP protection...

alex95 by Associate II
  • 478 Views
  • 2 replies
  • 3 kudos

Secure Boot research

Can you help with new research on secure boot?   I am a cyber security researcher at the University of Bristol in the UK. I would like to your views on Secure boot.   My area of interest is developer-centred security, specifically in the issues that ...

fe23957 by Associate
  • 274 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H503 cannot perform regression

Hello.  I am experimenting with securing a STM32H503 using password authentication, which will ultimately be an automated process.I created a simple password for testing and created the password hash in board_password.bin and da_password.bin(just for...

RGari by Associate III
  • 6902 Views
  • 28 replies
  • 0 kudos

Legacy SBSFU KMS on an STM32F4

I have legacy SBSFU based system running on an stm32f429 for a few years now, based on the STM32F413ZHT6 demo code that was present in the package. I am now interesting to using the KMS feature of SBSFU but after reading um2622 /seeing https://www.yo...

BPeet.1 by Associate
  • 488 Views
  • 1 replies
  • 0 kudos

Integrating TouchGFX and SBSFU

I am trying to integrate a very simple TouchGFX Application into the SBSFU (I only really need SB right now) application, on STM32U5A9J-DKI've switched out the Nonsecure application for mine, I've modified flash_layout to do primary only, no external...

JoeMck by Associate II
  • 609 Views
  • 3 replies
  • 0 kudos

Resolved! Correct forum for MOOC - Security?

I've been watching the MOOC - Security series and had some questions.  There is a link in the info block to a forum for any questions, but the link no longer works.  https://www.youtube.com/watch?v=g7ykhnmh7sAIs this the right place?I got to the end ...

KDesr.1 by Associate III
  • 381 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.