STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H753 Flash CRC address limitations

Hi,Although not specified in the reference manual it looks like the CRC process within the FLASH module (see section 4.3.12) has to have start and end addresses aligned to possibly the CRC_BURST size (I've only tried 128 byte bursts so far). If not a...

NPato by Associate III
  • 1832 Views
  • 2 replies
  • 0 kudos

STM32F765 - it has HW crypto or not?

On the pagehttps://www.st.com/en/microcontrollers-microprocessors/stm32f7x5.htmllegend says that STM32F765 has HW crypto (dark blue color). However datasheet and reference manual do not confirm that. Reference manual RM0410 says that 77xxx models hav...

BDurs by Associate II
  • 1632 Views
  • 1 replies
  • 0 kudos

stm32f429 x-cube-cryptolib import blank project

hello i try to test xcube-cryptolib rsa in blank project , my develop board stm32f429 disc1 and i added all lib files when i try to build get error justcollect2.exe: error: ld returned 1 exit statusmake: *** [makefile:44: test.elf] Error 1i cant unde...

tsah.1 by Associate
  • 906 Views
  • 0 replies
  • 1 kudos

Porting SBSFU to the same family

I'm trying port the SBSFU example STM32L476 board to our MCU which is STM32L475. Fortunately they are very similar. I'm going through the code and it makes sense but I could not find a single reference about porting it. ST has documents that explain ...

MHoss.1 by Associate III
  • 3172 Views
  • 6 replies
  • 0 kudos

CRC data ignored after CRC reset - revisited

I've been just bitten by https://community.st.com/s/feed/0D50X00009XkW6NSAV . [reconstructed] In an already proven working piece of code, I first check if an array's first word is equal to a constant (signature), then I reset the CRC and then feed it...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.